<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kinetis KM35 UART Transmission buffer control of RTS in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1485929#M63523</link>
    <description>&lt;P&gt;Thank you for all your guidance.&lt;/P&gt;&lt;P&gt;I am using KM35(MKM35Z512VLL7R)&lt;BR /&gt;I have a question about the RTS control during UART transmission.&lt;/P&gt;&lt;P&gt;As shown in the figure, the RTS that allows the transmit buffer, when observed on an oscilloscope&lt;BR /&gt;It appears to rise one bit before the data to be transmitted.&lt;BR /&gt;When transmission is completed, it also appears to fall one bit later.&lt;BR /&gt;My questions are the following two points.&lt;BR /&gt;(1) Does the time for this one bit change according to the baud rate?&lt;BR /&gt;(2) Is there any description of this specification?　I looked in the reference manual but could not understand.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Jul 2022 05:27:33 GMT</pubDate>
    <dc:creator>jun1</dc:creator>
    <dc:date>2022-07-07T05:27:33Z</dc:date>
    <item>
      <title>kinetis KM35 UART Transmission buffer control of RTS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1485929#M63523</link>
      <description>&lt;P&gt;Thank you for all your guidance.&lt;/P&gt;&lt;P&gt;I am using KM35(MKM35Z512VLL7R)&lt;BR /&gt;I have a question about the RTS control during UART transmission.&lt;/P&gt;&lt;P&gt;As shown in the figure, the RTS that allows the transmit buffer, when observed on an oscilloscope&lt;BR /&gt;It appears to rise one bit before the data to be transmitted.&lt;BR /&gt;When transmission is completed, it also appears to fall one bit later.&lt;BR /&gt;My questions are the following two points.&lt;BR /&gt;(1) Does the time for this one bit change according to the baud rate?&lt;BR /&gt;(2) Is there any description of this specification?　I looked in the reference manual but could not understand.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 05:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1485929#M63523</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2022-07-07T05:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: kinetis KM35 UART Transmission buffer control of RTS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1486439#M63537</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In order to have in the same channel, Do you read the chapter&amp;nbsp;&lt;STRONG&gt;45.5.1.7 Transceiver driver enable&lt;/STRONG&gt;, from the RM&amp;nbsp;and do not understand?&lt;/P&gt;
&lt;P&gt;I review the RM and in the UARTx_MODEM[RXRTSE] the assertion is controlled by this, and this will change depending on the baud rate.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 23:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1486439#M63537</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-07-07T23:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: kinetis KM35 UART Transmission buffer control of RTS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1487720#M63559</link>
      <description>&lt;P&gt;Thank you very much. I understand.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 01:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KM35-UART-Transmission-buffer-control-of-RTS/m-p/1487720#M63559</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2022-07-12T01:38:24Z</dc:date>
    </item>
  </channel>
</rss>