<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: power consumption when executing out of SRAM in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1482966#M63495</link>
    <description>&lt;P&gt;Which evaluation board are you using?&lt;/P&gt;</description>
    <pubDate>Thu, 30 Jun 2022 17:28:01 GMT</pubDate>
    <dc:creator>CarlosGarabito</dc:creator>
    <dc:date>2022-06-30T17:28:01Z</dc:date>
    <item>
      <title>power consumption when executing out of SRAM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1480023#M63450</link>
      <description>&lt;P&gt;i have a very-low power application which (conveniently) can fit entirely in SRAM....&lt;/P&gt;&lt;P&gt;in general, what's the cost of executing out of on-chip FLASH versus on-chip SRAM???&amp;nbsp; feel free to reference any specific kinetis device (cortex M0+ preferred) as an example....&lt;/P&gt;&lt;P&gt;i assume i'm already powering the SRAM; and i know that FLASH is often put into "doze" mode when in VLLSx...&amp;nbsp; it just wasn't obvious from any of the data sheets how much power (uA/mHz) the FLASH itself consumes when the processor is active....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 25 Jun 2022 00:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1480023#M63450</guid>
      <dc:creator>biosbob</dc:creator>
      <dc:date>2022-06-25T00:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: power consumption when executing out of SRAM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1482966#M63495</link>
      <description>&lt;P&gt;Which evaluation board are you using?&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 17:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1482966#M63495</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-06-30T17:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: power consumption when executing out of SRAM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1483072#M63502</link>
      <description>&lt;P&gt;i'm using several different boards, including the FRDM-KW38....&lt;/P&gt;&lt;P&gt;as i was looking through the datasheets of some LPC (cortex-m0+) parts, they all had a coremark score for SRAM and FLASH at different clock speeds....&amp;nbsp; on the LPC51U68, for instance, they quoted 62uA/MHz (SRAM) and 78uA/MHz (FLASH) with a 48 MHz clock....&amp;nbsp; the ratio between SRAM and FLASH was roughly the same at other clock speeds....&lt;/P&gt;&lt;P&gt;at this time, i'm looking for high-level confirmation that i would see similar improvement on comparable kintetis MCUs....&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 00:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1483072#M63502</guid>
      <dc:creator>biosbob</dc:creator>
      <dc:date>2022-07-01T00:51:03Z</dc:date>
    </item>
    <item>
      <title>Re: power consumption when executing out of SRAM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1484103#M63508</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/121550"&gt;@biosbob&lt;/a&gt;&amp;nbsp; &lt;SPAN&gt;I'd highly recommend you to refer to the application note &lt;/SPAN&gt;&lt;SPAN&gt;which illustrates the system performance running on the different memory devices (&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12437.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12437.pdf&lt;/A&gt;).&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 14:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/power-consumption-when-executing-out-of-SRAM/m-p/1484103#M63508</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-07-04T14:06:41Z</dc:date>
    </item>
  </channel>
</rss>