<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV4x PWM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1480785#M63466</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;In a nutshell, PWMA allows you to increase the resolution of the PWM signal.&lt;/P&gt;
&lt;P&gt;Regarding your second question, you can take as reference the application note &lt;A title="Sensorless PMSM Field-Oriented Control on Kinetis KV and KE" href="https://www.nxp.com/docs/en/application-note/AN5237.pdf" target="_blank" rel="noopener"&gt;AN5237&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;I hope this will help you.&lt;/P&gt;</description>
    <pubDate>Mon, 27 Jun 2022 22:27:48 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2022-06-27T22:27:48Z</dc:date>
    <item>
      <title>KV4x PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1480332#M63462</link>
      <description>&lt;P&gt;In KV4x Reference Manual there are two options to generate PWM&lt;/P&gt;&lt;P&gt;Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)&lt;/P&gt;&lt;P&gt;Chapter 39 : FlexTimer Module (FTM)&lt;/P&gt;&lt;P&gt;what is the difference between these two..??&lt;/P&gt;&lt;P&gt;with both i can successfully&amp;nbsp; able to generate complimentary pwm signals with deadtime insertion for my full bridge power supply application.&lt;/P&gt;&lt;P&gt;I aslo need to read CADC.&lt;/P&gt;&lt;P&gt;found the document for "&amp;nbsp;FlexTimer and ADC Synchronization for Field Oriented Control on Kinetis ".&lt;/P&gt;&lt;P&gt;is it possible to use ADC in sync with PWM(Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)) .....same as&amp;nbsp;FlexTimer..?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 06:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1480332#M63462</guid>
      <dc:creator>Vishesh45</dc:creator>
      <dc:date>2022-06-27T06:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1480785#M63466</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;In a nutshell, PWMA allows you to increase the resolution of the PWM signal.&lt;/P&gt;
&lt;P&gt;Regarding your second question, you can take as reference the application note &lt;A title="Sensorless PMSM Field-Oriented Control on Kinetis KV and KE" href="https://www.nxp.com/docs/en/application-note/AN5237.pdf" target="_blank" rel="noopener"&gt;AN5237&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;I hope this will help you.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 22:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1480785#M63466</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-06-27T22:27:48Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1487222#M63547</link>
      <description>&lt;P&gt;.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 04:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1487222#M63547</guid>
      <dc:creator>Vishesh45</dc:creator>
      <dc:date>2022-08-03T04:28:52Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1499951#M63725</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank you for your&amp;nbsp;&lt;STRONG&gt;response&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;valuable&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;suggestion&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;of application note AN5237, with the help of that i have&amp;nbsp;&lt;SPAN&gt;successfully&amp;nbsp;sync ADC with&amp;nbsp;PWMA/eFlexPWM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As you have mentioned in above comment "&lt;STRONG&gt;PWMA allows you to increase the resolution of the PWM signal&lt;/STRONG&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have found(on NXP site) and referd document&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Nano-edge-placement-feature-for-eFlexPWM-module-based-on-KV4x/ta-p/1105571" target="_blank" rel="noopener"&gt;Nano-edge placement of eFlexPWM on KV4x family&lt;/A&gt;&amp;nbsp;&lt;STRONG&gt;.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;As per the document it helps to increse duty cycle resolution by using fractional unit, so we can have duty cycle like&amp;nbsp;50.03125,&lt;BR /&gt;50.0625, 50.09325,50.125,…….50.96875.&lt;/P&gt;&lt;P&gt;my quary is regarding&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;frequency resolution&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;in my application i have to use fix 50% duty cyle and have to change frquency as per the need.&lt;/P&gt;&lt;P&gt;Example :&amp;nbsp;e PWM driving clock for KV4x is 100MHz&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Total Timer Ticks : 1000 will generate frq 100000 Hz (100KHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Total Timer Ticks : 999 will generate frq 100100.1001001001 Hz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;so 1 tick will produce 100Hz diffrance...and this diffrance increase as we go higher in frquency.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it possible to&amp;nbsp;increase frquency resolution using fractional unit.??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;orr it is just helps with duty cycle..??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;in my application i need to vary frquency in range from 45KHz to 100KHz. I have no idea right now how much resolution i required but if it is possible to increase&amp;nbsp;resolution like in duty cycle..,,,would like to go for it for&amp;nbsp;precise performance.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 04:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1499951#M63725</guid>
      <dc:creator>Vishesh45</dc:creator>
      <dc:date>2022-08-03T04:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1500339#M63732</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/54510"&gt;@Vishesh45&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for continuing to use our community.&lt;/P&gt;
&lt;P&gt;This case has already been closed and marked as solved. Could you please open a new case with this new question in order to continue giving you support? This is also for the purpose of having a better Q&amp;amp;A follow-up.&lt;/P&gt;
&lt;P&gt;Thank you in advance. Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 14:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-PWM/m-p/1500339#M63732</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-08-03T14:48:20Z</dc:date>
    </item>
  </channel>
</rss>