<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 PWMA/eFlexPWM Vs FlexTimer Module in KV4x</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWMA-eFlexPWM-Vs-FlexTimer-Module-in-KV4x/m-p/1480084#M63459</link>
    <description>&lt;P&gt;In KV4x Reference Manual there are two options to generate PWM&lt;/P&gt;&lt;P&gt;Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)&lt;/P&gt;&lt;P&gt;Chapter 39 : FlexTimer Module (FTM)&lt;/P&gt;&lt;P&gt;what is the difference between these two..??&lt;/P&gt;&lt;P&gt;with both i can successfully&amp;nbsp; able to generate complimentary pwm signals with deadtime insertion for my full bridge power supply application.&lt;/P&gt;&lt;P&gt;I aslo need to read CADC.&lt;/P&gt;&lt;P&gt;found the document for "&amp;nbsp;FlexTimer and ADC Synchronization for Field Oriented Control on Kinetis ".&lt;/P&gt;&lt;P&gt;is it possible to use ADC in sync with PWM(Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)) .....same as&amp;nbsp;FlexTimer..?&lt;/P&gt;</description>
    <pubDate>Sat, 25 Jun 2022 17:30:41 GMT</pubDate>
    <dc:creator>Vishesh45</dc:creator>
    <dc:date>2022-06-25T17:30:41Z</dc:date>
    <item>
      <title>PWMA/eFlexPWM Vs FlexTimer Module in KV4x</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWMA-eFlexPWM-Vs-FlexTimer-Module-in-KV4x/m-p/1480084#M63459</link>
      <description>&lt;P&gt;In KV4x Reference Manual there are two options to generate PWM&lt;/P&gt;&lt;P&gt;Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)&lt;/P&gt;&lt;P&gt;Chapter 39 : FlexTimer Module (FTM)&lt;/P&gt;&lt;P&gt;what is the difference between these two..??&lt;/P&gt;&lt;P&gt;with both i can successfully&amp;nbsp; able to generate complimentary pwm signals with deadtime insertion for my full bridge power supply application.&lt;/P&gt;&lt;P&gt;I aslo need to read CADC.&lt;/P&gt;&lt;P&gt;found the document for "&amp;nbsp;FlexTimer and ADC Synchronization for Field Oriented Control on Kinetis ".&lt;/P&gt;&lt;P&gt;is it possible to use ADC in sync with PWM(Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)) .....same as&amp;nbsp;FlexTimer..?&lt;/P&gt;</description>
      <pubDate>Sat, 25 Jun 2022 17:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWMA-eFlexPWM-Vs-FlexTimer-Module-in-KV4x/m-p/1480084#M63459</guid>
      <dc:creator>Vishesh45</dc:creator>
      <dc:date>2022-06-25T17:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: PWMA/eFlexPWM Vs FlexTimer Module in KV4x</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWMA-eFlexPWM-Vs-FlexTimer-Module-in-KV4x/m-p/1480786#M63467</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that you have another case with the same question, I will follow up on this last one that I mention.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 22:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWMA-eFlexPWM-Vs-FlexTimer-Module-in-KV4x/m-p/1480786#M63467</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-06-27T22:27:30Z</dc:date>
    </item>
  </channel>
</rss>