<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can I share bootloaders between MCUs? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1473895#M63336</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160985"&gt;@derekcook&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I’m afraid this isn’t possible.&lt;/P&gt;&lt;P&gt;Even though they are both MCUs from the same series, the differences between these two MCUs wouldn’t allow them to share bootloaders.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Tue, 14 Jun 2022 21:37:19 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2022-06-14T21:37:19Z</dc:date>
    <item>
      <title>Can I share bootloaders between MCUs?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1473821#M63325</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to use a bootloader developed for the KV31 with the KV56?&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 17:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1473821#M63325</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2022-06-14T17:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: Can I share bootloaders between MCUs?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1473895#M63336</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160985"&gt;@derekcook&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I’m afraid this isn’t possible.&lt;/P&gt;&lt;P&gt;Even though they are both MCUs from the same series, the differences between these two MCUs wouldn’t allow them to share bootloaders.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 21:37:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1473895#M63336</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-06-14T21:37:19Z</dc:date>
    </item>
    <item>
      <title>Re: Can I share bootloaders between MCUs?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1474664#M63347</link>
      <description>&lt;P&gt;It looks like there is not a MCUBOOT specifically for the&amp;nbsp;&lt;SPAN&gt;MKV56F512xxx24. However, there is a bootloader for the KV58F220M. I assume that's because this same bootloader works with the MKV56?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 19:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1474664#M63347</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2022-06-15T19:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: Can I share bootloaders between MCUs?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1474694#M63348</link>
      <description>&lt;P&gt;I am following this document to port the KV58F220M bootloader to the KV56.&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/reference-manual/MCUBOOTRM.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/MCUBOOTRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;With the KV31 we had our bootloader load to flash at 0xA000. We can still load to the same flash location with KV56? I noticed the default location was&amp;nbsp;0x1000a000.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 19:53:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1474694#M63348</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2022-06-15T19:53:33Z</dc:date>
    </item>
    <item>
      <title>Re: Can I share bootloaders between MCUs?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1474696#M63349</link>
      <description>&lt;P&gt;I see RAM is at 0x0000 to 0x10000. Is this fixed? If so I guess my bootloader must be from 0x10000000 to&amp;nbsp;0x1000a000 and my application can start at&amp;nbsp;0x1000a000&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="derekcook_0-1655322896756.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183508iBDC2E085F55F1FF8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="derekcook_0-1655322896756.png" alt="derekcook_0-1655322896756.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;derekcook_0-1655322896756.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 19:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1474696#M63349</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2022-06-15T19:56:50Z</dc:date>
    </item>
    <item>
      <title>Re: Can I share bootloaders between MCUs?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1476927#M63400</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160985"&gt;@derekcook&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You are correct. The RAM address is fixed, but the code address starts at 0x1000_0000. Table 5-1 of the datasheet shows the Memory Map:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EdwinHz_0-1655742801339.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183928i34FE9FB49B217B66/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EdwinHz_0-1655742801339.png" alt="EdwinHz_0-1655742801339.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EdwinHz_0-1655742801339.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 16:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-share-bootloaders-between-MCUs/m-p/1476927#M63400</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-06-20T16:34:54Z</dc:date>
    </item>
  </channel>
</rss>