<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC Timer Trigger in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Timer-Trigger/m-p/1470108#M63264</link>
    <description>&lt;P&gt;Hello everybody!&lt;/P&gt;&lt;P&gt;I want to trigger an ADC measurement with a timer event (OnCounterRestart) and actually it should be straight forward, but I do not get it working.&lt;/P&gt;&lt;P&gt;I'm working with Kinetis Design Studio, because my MCU isn't supported by the newer IDEA from NXP. Attached you can find a processor expert project with the minimal amount of components which should do the job. The code is based on the "Typical Usage" examples in the help window of the ADC-component. I set the Trigger input to Flex_timer_0 and created a new TimerUnit_LDD component which should initiate the ADC-measurement. Do i need to setup the timer in a specific way too?&lt;/P&gt;&lt;P&gt;I'm grateful for any help! Thank you in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 07 Jun 2022 16:27:24 GMT</pubDate>
    <dc:creator>SimonS</dc:creator>
    <dc:date>2022-06-07T16:27:24Z</dc:date>
    <item>
      <title>ADC Timer Trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Timer-Trigger/m-p/1470108#M63264</link>
      <description>&lt;P&gt;Hello everybody!&lt;/P&gt;&lt;P&gt;I want to trigger an ADC measurement with a timer event (OnCounterRestart) and actually it should be straight forward, but I do not get it working.&lt;/P&gt;&lt;P&gt;I'm working with Kinetis Design Studio, because my MCU isn't supported by the newer IDEA from NXP. Attached you can find a processor expert project with the minimal amount of components which should do the job. The code is based on the "Typical Usage" examples in the help window of the ADC-component. I set the Trigger input to Flex_timer_0 and created a new TimerUnit_LDD component which should initiate the ADC-measurement. Do i need to setup the timer in a specific way too?&lt;/P&gt;&lt;P&gt;I'm grateful for any help! Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 16:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Timer-Trigger/m-p/1470108#M63264</guid>
      <dc:creator>SimonS</dc:creator>
      <dc:date>2022-06-07T16:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Timer Trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Timer-Trigger/m-p/1470867#M63283</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Unfortunately, the KDS IDE does not have support, I recommend using the MCUXpresso and you can download de SDK from TWRK21D50 to see the example and export it to your device.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 18:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Timer-Trigger/m-p/1470867#M63283</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-06-08T18:04:54Z</dc:date>
    </item>
  </channel>
</rss>