<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KV4x: ENC driver</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1468569#M63236</link>
    <description>&lt;P&gt;How do I do this exactly? There is only one output of this module: POSMATCH.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Fri, 03 Jun 2022 07:25:48 GMT</pubDate>
    <dc:creator>lenoirlaw</dc:creator>
    <dc:date>2022-06-03T07:25:48Z</dc:date>
    <item>
      <title>KV4x: ENC driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1463098#M63155</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am new to the field of embedded systems. I have a MKV46F16 µC on a board. I have to connect an encoder and implement a module to get the position and speed of a motor. The problem is that I only have the PTC4...PTC7 pins available. The FTM1 has a Quadrature decoder feature, but the specific pins are not at PTC4...PTC7. So unfortunately i can't use the FTM module.&amp;nbsp; For this reason I use the ENC module, but I can't find the timer register to get timestamps to determine the speed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the best way to proceed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance and best regards,&lt;/P&gt;&lt;P&gt;lenoirlaw&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 09:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1463098#M63155</guid>
      <dc:creator>lenoirlaw</dc:creator>
      <dc:date>2022-05-24T09:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x: ENC driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1466396#M63197</link>
      <description>&lt;P&gt;Hi Lenoirlaw,&lt;/P&gt;&lt;P&gt;You can connect signals of this module to a general purpose timer to make speed velocity measurements.&lt;/P&gt;&lt;P&gt;Wish it helps you. If you still have questions about it, please kindly let me know.&lt;/P&gt;</description>
      <pubDate>Mon, 30 May 2022 22:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1466396#M63197</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-05-30T22:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x: ENC driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1468569#M63236</link>
      <description>&lt;P&gt;How do I do this exactly? There is only one output of this module: POSMATCH.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jun 2022 07:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1468569#M63236</guid>
      <dc:creator>lenoirlaw</dc:creator>
      <dc:date>2022-06-03T07:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x: ENC driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1469544#M63253</link>
      <description>&lt;P&gt;Hi Lenoirlaw,&lt;/P&gt;
&lt;P&gt;The RT1050 has a similar or even the same module. In its reference manual, it explains the speed measurement method in more detail (Please see section 55.3.4 Speed Measurement Method).&lt;/P&gt;
&lt;P&gt;&lt;A title="i.MX RT1050 Processor Reference Manual" href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_blank" rel="noopener"&gt;i.MX RT1050 Processor Reference Manual&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope it helps you. If you still have questions about it, please let me know.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jun 2022 21:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1469544#M63253</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-06-06T21:44:41Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x: ENC driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1470170#M63269</link>
      <description>&lt;P&gt;This will not work for my case, because the KV4x does not support the registers LASTEDGEH and POSDPERH.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 20:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1470170#M63269</guid>
      <dc:creator>lenoirlaw</dc:creator>
      <dc:date>2022-06-07T20:45:48Z</dc:date>
    </item>
    <item>
      <title>Re: KV4x: ENC driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1470976#M63284</link>
      <description>&lt;P&gt;Apologies. That's correct, the KV4x does not support these registers.&lt;/P&gt;
&lt;P&gt;In such a case, you will need to create an algorithm using a general purpose timer as the time base connected to the TRIGGER and take a snapshot of the POSD register in order to calculate speed. Wish it helps you.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 20:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV4x-ENC-driver/m-p/1470976#M63284</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-06-08T20:32:16Z</dc:date>
    </item>
  </channel>
</rss>