<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKEAZ64 Disable NMI</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-Disable-NMI/m-p/1467134#M63206</link>
    <description>&lt;P&gt;could i disable the NMI interrupt&amp;nbsp; &lt;SPAN class=""&gt;after system reset&lt;/SPAN&gt;&amp;nbsp;，before into the main function.&lt;/P&gt;&lt;P&gt;like change the flash data or something else.&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 01 Jun 2022 03:47:11 GMT</pubDate>
    <dc:creator>1915135412</dc:creator>
    <dc:date>2022-06-01T03:47:11Z</dc:date>
    <item>
      <title>KEAZ64 Disable NMI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-Disable-NMI/m-p/1467134#M63206</link>
      <description>&lt;P&gt;could i disable the NMI interrupt&amp;nbsp; &lt;SPAN class=""&gt;after system reset&lt;/SPAN&gt;&amp;nbsp;，before into the main function.&lt;/P&gt;&lt;P&gt;like change the flash data or something else.&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 03:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-Disable-NMI/m-p/1467134#M63206</guid>
      <dc:creator>1915135412</dc:creator>
      <dc:date>2022-06-01T03:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: KEAZ64 Disable NMI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-Disable-NMI/m-p/1467455#M63212</link>
      <description>&lt;P&gt;By definition Non Maskable Interrupts can not be disabled at run time.&lt;BR /&gt;&lt;BR /&gt;Many parts do have a Flash configuration option byte that will either disable NMI completely before executing code or turn it into an alternative function such as enabling the bootloader.&lt;BR /&gt;&lt;BR /&gt;Regardless of that, any NMI pin must not be asserted at reset or allowed to float.&lt;BR /&gt;There can be timing races in some parts that cause the NMI to happen before anything else.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 12:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-Disable-NMI/m-p/1467455#M63212</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2022-06-01T12:16:49Z</dc:date>
    </item>
  </channel>
</rss>