<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: WDOG_CS not showing correct value in debug mode using Jlink</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1462136#M63148</link>
    <description>&lt;P&gt;Yes I am trying to read through code. At startup, the register view for WDOG_CS is shared in the image. But the reset value of the register should be 0x2980(As per datasheet).&lt;/P&gt;</description>
    <pubDate>Mon, 23 May 2022 05:40:07 GMT</pubDate>
    <dc:creator>MithileshKumar</dc:creator>
    <dc:date>2022-05-23T05:40:07Z</dc:date>
    <item>
      <title>WDOG_CS not showing correct value in debug mode using Jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1461665#M63141</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using MKE15Z series MCU. As per datasheet the default value of WDOG_CS should be 0x2980 but what obtained is 0x420 which is incorrect. But with CMSIS-DAP getting the correct value.&lt;/P&gt;&lt;P&gt;Is it related to debugger. If yes, is there any workaround for this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 13:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1461665#M63141</guid>
      <dc:creator>MithileshKumar</dc:creator>
      <dc:date>2022-05-20T13:21:13Z</dc:date>
    </item>
    <item>
      <title>Re: WDOG_CS not showing correct value in debug mode using Jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1462028#M63147</link>
      <description>&lt;P&gt;Hi&amp;nbsp;MithileshKumar,&lt;/P&gt;
&lt;P&gt;Did you try to read the value of WDOG_CS through code? Check if the value is the same as the debugger register view?&lt;/P&gt;
&lt;P&gt;If you still have problems after updating the J-Link software, it is recommended to submit a technical service request to &lt;A href="https://www.segger.com/support/technical-support/" target="_self"&gt;SEGGER&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 02:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1462028#M63147</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-05-23T02:16:38Z</dc:date>
    </item>
    <item>
      <title>Re: WDOG_CS not showing correct value in debug mode using Jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1462136#M63148</link>
      <description>&lt;P&gt;Yes I am trying to read through code. At startup, the register view for WDOG_CS is shared in the image. But the reset value of the register should be 0x2980(As per datasheet).&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 05:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/WDOG-CS-not-showing-correct-value-in-debug-mode-using-Jlink/m-p/1462136#M63148</guid>
      <dc:creator>MithileshKumar</dc:creator>
      <dc:date>2022-05-23T05:40:07Z</dc:date>
    </item>
  </channel>
</rss>