<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Extracting code stored in FRDM-K64F-ND</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Extracting-code-stored-in-FRDM-K64F-ND/m-p/1453706#M63043</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've recently been given a project to rebuild a system made with a FRDM-K64F-ND board, but the issue is that there are jumper wires missing from the assembly and working with an oscilloscope to find which pin provides the output has been fruitless. I was hoping to find a way to extract the code already uploaded on the board to see which pin's are included in it. I'm a biomedical engineering student so I haven't worked with coding this in depth before and any help would be appreciated!&lt;/P&gt;</description>
    <pubDate>Thu, 05 May 2022 17:09:31 GMT</pubDate>
    <dc:creator>Gaul567</dc:creator>
    <dc:date>2022-05-05T17:09:31Z</dc:date>
    <item>
      <title>Extracting code stored in FRDM-K64F-ND</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Extracting-code-stored-in-FRDM-K64F-ND/m-p/1453706#M63043</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've recently been given a project to rebuild a system made with a FRDM-K64F-ND board, but the issue is that there are jumper wires missing from the assembly and working with an oscilloscope to find which pin provides the output has been fruitless. I was hoping to find a way to extract the code already uploaded on the board to see which pin's are included in it. I'm a biomedical engineering student so I haven't worked with coding this in depth before and any help would be appreciated!&lt;/P&gt;</description>
      <pubDate>Thu, 05 May 2022 17:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Extracting-code-stored-in-FRDM-K64F-ND/m-p/1453706#M63043</guid>
      <dc:creator>Gaul567</dc:creator>
      <dc:date>2022-05-05T17:09:31Z</dc:date>
    </item>
  </channel>
</rss>