<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXpresso IDE Timers List not working in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444654#M62904</link>
    <description>&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;Thank you so much for the answer.&lt;/P&gt;&lt;P&gt;i am using Segger JLINK plus, and have to pause the IDE to view variables or RTOS information (task, queue, etc).&amp;nbsp; i am trying to see real time update RTOS information (heap, task, queue, etc) while IDE is "not" paused.&amp;nbsp; Can you please let me know which probe to do so or which IDE setting that you have experienced?&lt;/P&gt;&lt;P&gt;for the timer, i have it defined and i know it is running because every time the timer expires, the call back function issue an even to run a task and i track the task is running. but still i can not see the timer in the Timers List, please see example below.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Henry&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="henrynguyen_0-1650039026569.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177079i9BF3D92835F109C4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="henrynguyen_0-1650039026569.png" alt="henrynguyen_0-1650039026569.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="henrynguyen_1-1650039050407.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177080i307BC49F7351683C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="henrynguyen_1-1650039050407.png" alt="henrynguyen_1-1650039050407.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 15 Apr 2022 16:11:43 GMT</pubDate>
    <dc:creator>henrynguyen</dc:creator>
    <dc:date>2022-04-15T16:11:43Z</dc:date>
    <item>
      <title>MCUXpresso IDE Timers List not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444315#M62900</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i am using MCUXpresso v11.4.1 (build 6260) with FreeRTOS for MK66&lt;/P&gt;&lt;P&gt;i can see the Heap Usage, Tasks, Queues, Instruction traces, but i can not see my timer under Timers List.&lt;/P&gt;&lt;P&gt;can you please let me know why?&lt;/P&gt;&lt;P&gt;also, i am using Jlink Pro, not sure why i can not do the non-stop debug?&lt;/P&gt;&lt;P&gt;for non-stop debug, what debugger should i use?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Henry&lt;/P&gt;</description>
      <pubDate>Thu, 14 Apr 2022 23:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444315#M62900</guid>
      <dc:creator>henrynguyen</dc:creator>
      <dc:date>2022-04-14T23:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE Timers List not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444412#M62901</link>
      <description>&lt;P&gt;You only need to worry about non-stop or full-stop mode if you are using LinkServer (see &lt;A href="https://mcuoneclipse.com/2019/01/13/gdb-all-stop-and-non-stop-mode-with-linkserver/" target="_blank"&gt;https://mcuoneclipse.com/2019/01/13/gdb-all-stop-and-non-stop-mode-with-linkserver/&lt;/A&gt;). J-Link works does not have (and need) such a setting.&lt;/P&gt;&lt;P&gt;I recommend that you have a read at &lt;A href="https://mcuoneclipse.com/2018/05/27/tutorial-understanding-and-using-freertos-software-timers/" target="_blank"&gt;https://mcuoneclipse.com/2018/05/27/tutorial-understanding-and-using-freertos-software-timers/&lt;/A&gt;: you only will see something in the timers list inside Eclipse if the timer is active or running. But you can see all the time the timer daemon task queue.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Fri, 15 Apr 2022 05:42:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444412#M62901</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-04-15T05:42:38Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE Timers List not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444654#M62904</link>
      <description>&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;Thank you so much for the answer.&lt;/P&gt;&lt;P&gt;i am using Segger JLINK plus, and have to pause the IDE to view variables or RTOS information (task, queue, etc).&amp;nbsp; i am trying to see real time update RTOS information (heap, task, queue, etc) while IDE is "not" paused.&amp;nbsp; Can you please let me know which probe to do so or which IDE setting that you have experienced?&lt;/P&gt;&lt;P&gt;for the timer, i have it defined and i know it is running because every time the timer expires, the call back function issue an even to run a task and i track the task is running. but still i can not see the timer in the Timers List, please see example below.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Henry&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="henrynguyen_0-1650039026569.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177079i9BF3D92835F109C4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="henrynguyen_0-1650039026569.png" alt="henrynguyen_0-1650039026569.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="henrynguyen_1-1650039050407.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177080i307BC49F7351683C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="henrynguyen_1-1650039050407.png" alt="henrynguyen_1-1650039050407.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Apr 2022 16:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1444654#M62904</guid>
      <dc:creator>henrynguyen</dc:creator>
      <dc:date>2022-04-15T16:11:43Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE Timers List not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1445560#M62911</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/128384"&gt;@henrynguyen&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;These views are stop-mode-views, so you have to halt/pause the target in order to view the data. They are using gdb expressions which only can be executed with the target paused.&lt;/P&gt;&lt;P&gt;As for your screenshots: I cannot see much because the files/resolution is too low.&lt;/P&gt;&lt;P&gt;Just as a general comment: you might try out the latest version 11.5.1 which just came out, in case you have an older one:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2022/04/19/mcuxpresso-ide-11-5-1/" target="_blank"&gt;https://mcuoneclipse.com/2022/04/19/mcuxpresso-ide-11-5-1/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 08:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-IDE-Timers-List-not-working/m-p/1445560#M62911</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-04-19T08:16:22Z</dc:date>
    </item>
  </channel>
</rss>