<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Connect FRDM-KEAZ128 to J-Link in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1440460#M62847</link>
    <description>&lt;P&gt;Sorry for the delay.&lt;BR /&gt;Please measure the voltage of Pin 1 and 3 without connect jumper of J107. Check if the voltage source is correct. If the voltage is correct before connect the jumper of J107, then you may need to check the circuit behind.(2v and 0v are all incorrect. J10 can select 3.3v or 5V, but it's default to 5V)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="J107 FRDM-KEA128 J16.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176224iA2799063EE1A00FD/image-size/large?v=v2&amp;amp;px=999" role="button" title="J107 FRDM-KEA128 J16.png" alt="J107 FRDM-KEA128 J16.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;J107 FRDM-KEA128 J16.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;What's the SCH version of your FRDM-KEAZ128? There should be a sticker on the bottom of the board that says SCH version.&lt;/P&gt;
&lt;P&gt;If OpenSDA is not powered(J7 not plug), then connect 2-3 of J104, press SW1 will hold low the RESET.&lt;BR /&gt;If OpenSDA is powered, then connect 1-2 of J104, the OpenSDA will output low to&amp;nbsp;RESET.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Apr 2022 09:44:10 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-04-07T09:44:10Z</dc:date>
    <item>
      <title>Connect FRDM-KEAZ128 to J-Link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1436535#M62804</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just received an FRDM-KEAZ128 board and am trying to connect via J-Link. The connection of different devices is attached. When I typed `&lt;FONT face="lucida sans unicode,lucida sans"&gt;connect&lt;/FONT&gt;` on the J-Link Commander, I received the following printout:&lt;/P&gt;&lt;P&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;SEGGER J-Link Commander V7.62c (Compiled Mar 23 2022 16:45:48)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;DLL version V7.62c, compiled Mar 23 2022 16:44:32&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Connecting to J-Link via USB...O.K.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Firmware: J-Link V11 compiled Mar 3 2022 10:16:14&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Hardware version: V11.00&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;S/N: 51022156&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;License(s): GDB&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;USB speed mode: Full speed (12 MBit/s)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;VTref=1.844V&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Type "connect" to establish a target connection, '?' for help&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;J-Link&amp;gt;connect&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Please specify device / core. &amp;lt;Default&amp;gt;: S9KEAZ128XXXX (ALLOW SECURITY)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Type '?' for selection dialog&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Please specify target interface:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;J) JTAG (Default)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;S) SWD&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;T) cJTAG&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;TIF&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device position in JTAG chain (IRPre,DRPre) &amp;lt;Default&amp;gt;: -1,-1 =&amp;gt; Auto-detect&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;JTAGConf&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Specify target interface speed [kHz]. &amp;lt;Default&amp;gt;: 4000 kHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Speed&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device "S9KEAZ128XXXX (ALLOW SECURITY)" selected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Connecting to target via JTAG&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;InitTarget()&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Connect Under Reset&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;For debugger connection the device needs to be unsecured.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Executing default behavior previously saved in the registry.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device will be unsecured now.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Timeout while unsecuring device. Erase never starts.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;InitTarget()&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Connect Under Reset&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;For debugger connection the device needs to be unsecured.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Executing default behavior previously saved in the registry.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device will be unsecured now.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Timeout while unsecuring device. Erase never starts.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;InitTarget()&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Connect Under Reset&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;For debugger connection the device needs to be unsecured.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Executing default behavior previously saved in the registry.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device will be unsecured now.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Timeout while unsecuring device. Erase never starts.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;InitTarget()&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Connect Under Reset&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;For debugger connection the device needs to be unsecured.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Executing default behavior previously saved in the registry.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Device will be unsecured now.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Timeout while unsecuring device. Erase never starts.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Cannot connect to target.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I shorted jumper wires 2 and 3, which is supposed to be the config "Reset signal direct to the MCU when OpenSDA is not powered". When I plugged in the power supply, I found green LED on D3 and red LED near SW1, and the LED D11 is not blinking. (This LED blinked when I shorted jumpers 1 and 2, so I think my board is functioning). However, when I checked voltage between GND (pin J3-13) and 5V (pin J3-09), I found the output to be 2.5V. Is this normal? Another thing that I found suspicious was that Vref to J-Link was 1.844V, but I suppose J-Link Vref is often 3.3V. Is this why my connection failed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Mar 2022 22:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1436535#M62804</guid>
      <dc:creator>laonia</dc:creator>
      <dc:date>2022-03-30T22:08:33Z</dc:date>
    </item>
    <item>
      <title>Re: Connect FRDM-KEAZ128 to J-Link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1436997#M62806</link>
      <description>&lt;P&gt;Hi&amp;nbsp;laonia,&lt;/P&gt;
&lt;P&gt;Since you power the board through J16 with external 12V, then the J107 should connect 1-2(SBC power P5V0). If still not able to connect the KEA with external Segger JLink, then please refer:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-error-while-accessing-MDM-AP/m-p/651153" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Communication error while accessing MDM-AP.&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 10:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1436997#M62806</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-03-31T10:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: Connect FRDM-KEAZ128 to J-Link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1437084#M62808</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;If I connect J107 1 and 2, then Vref at SDA/JTAG is 0V. Is this normal? Because of this low voltage, I got an error saying&amp;nbsp;&lt;FONT face="lucida sans unicode,lucida sans" size="2"&gt;Target voltage too low.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I also had a warning saying&amp;nbsp;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;&lt;FONT face="lucida sans unicode,lucida sans"&gt;RESET (pin 15) high, but should be low. Please check target hardware&amp;nbsp;&lt;/FONT&gt;&lt;/FONT&gt;while pressing down the reset button and powering up the board. Is this the correct way to set RESET to low?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 13:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1437084#M62808</guid>
      <dc:creator>laonia</dc:creator>
      <dc:date>2022-03-31T13:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: Connect FRDM-KEAZ128 to J-Link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1440460#M62847</link>
      <description>&lt;P&gt;Sorry for the delay.&lt;BR /&gt;Please measure the voltage of Pin 1 and 3 without connect jumper of J107. Check if the voltage source is correct. If the voltage is correct before connect the jumper of J107, then you may need to check the circuit behind.(2v and 0v are all incorrect. J10 can select 3.3v or 5V, but it's default to 5V)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="J107 FRDM-KEA128 J16.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176224iA2799063EE1A00FD/image-size/large?v=v2&amp;amp;px=999" role="button" title="J107 FRDM-KEA128 J16.png" alt="J107 FRDM-KEA128 J16.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;J107 FRDM-KEA128 J16.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;What's the SCH version of your FRDM-KEAZ128? There should be a sticker on the bottom of the board that says SCH version.&lt;/P&gt;
&lt;P&gt;If OpenSDA is not powered(J7 not plug), then connect 2-3 of J104, press SW1 will hold low the RESET.&lt;BR /&gt;If OpenSDA is powered, then connect 1-2 of J104, the OpenSDA will output low to&amp;nbsp;RESET.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 09:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-FRDM-KEAZ128-to-J-Link/m-p/1440460#M62847</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-04-07T09:44:10Z</dc:date>
    </item>
  </channel>
</rss>