<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCUxpresso Ide configuration for USB CDC in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUxpresso-Ide-configuration-for-USB-CDC/m-p/1431246#M62694</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to run a USB CDC example for MKL27Z64LH4 in Windows 10.&amp;nbsp; I debug the code with JLink EDU but I didn't get any output. I think I have to configure MUCxpresso Ide to run the code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;How do I need to configure the IDE? e.g. clocks, peripherals, and pins.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MKL27Z64LH4 datasheet says it supports&amp;nbsp;USB FS 2.0 but I am using USB 3.0, is there any problem?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance. I will be really thankful if anyone helps me with this problem as it is part of my master's thesis.&lt;/P&gt;&lt;P&gt;RADUAN&lt;/P&gt;</description>
    <pubDate>Mon, 21 Mar 2022 10:21:22 GMT</pubDate>
    <dc:creator>raduansarif</dc:creator>
    <dc:date>2022-03-21T10:21:22Z</dc:date>
    <item>
      <title>MCUxpresso Ide configuration for USB CDC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUxpresso-Ide-configuration-for-USB-CDC/m-p/1431246#M62694</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to run a USB CDC example for MKL27Z64LH4 in Windows 10.&amp;nbsp; I debug the code with JLink EDU but I didn't get any output. I think I have to configure MUCxpresso Ide to run the code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;How do I need to configure the IDE? e.g. clocks, peripherals, and pins.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MKL27Z64LH4 datasheet says it supports&amp;nbsp;USB FS 2.0 but I am using USB 3.0, is there any problem?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance. I will be really thankful if anyone helps me with this problem as it is part of my master's thesis.&lt;/P&gt;&lt;P&gt;RADUAN&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 10:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUxpresso-Ide-configuration-for-USB-CDC/m-p/1431246#M62694</guid>
      <dc:creator>raduansarif</dc:creator>
      <dc:date>2022-03-21T10:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: MCUxpresso Ide configuration for USB CDC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUxpresso-Ide-configuration-for-USB-CDC/m-p/1431365#M62700</link>
      <description>&lt;P&gt;What exactly does this part mean?:&lt;/P&gt;&lt;P&gt;"&lt;STRONG&gt;MKL27Z64LH4 datasheet says it supports&amp;nbsp;USB FS 2.0 but I am using USB 3.0, is there any problem?"&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;If you are asking can up plug the 27Z into a blue USB 3.0 Type-A port, the answer is yes.&lt;BR /&gt;If you mean something else, the answer is no.&lt;BR /&gt;&lt;BR /&gt;Take a look here:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://hackaday.com/2022/03/07/a-chip-to-address-the-fundamental-usb-3-0-deficiency/" target="_blank"&gt;https://hackaday.com/2022/03/07/a-chip-to-address-the-fundamental-usb-3-0-deficiency/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It may be easier to get TinyUSB running, as there is a KL25 example. Difference to the KL27 is t&amp;nbsp;mostly initialization.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.tinyusb.org" target="_blank"&gt;https://www.tinyusb.org&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 14:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUxpresso-Ide-configuration-for-USB-CDC/m-p/1431365#M62700</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2022-03-21T14:35:31Z</dc:date>
    </item>
  </channel>
</rss>