<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: OTAP about hrs by example on KW36</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OTAP-about-hrs-by-example-on-KW36/m-p/1425781#M62589</link>
    <description>&lt;P&gt;solved.because the bootloader has been modified by other man,so after change the bootloader back to "bootloader_otap_frdmkw36.bin",it works&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 03:34:47 GMT</pubDate>
    <dc:creator>yeyue</dc:creator>
    <dc:date>2022-03-10T03:34:47Z</dc:date>
    <item>
      <title>OTAP about hrs by example on KW36</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OTAP-about-hrs-by-example-on-KW36/m-p/1424853#M62577</link>
      <description>&lt;P&gt;hi ,&lt;/P&gt;&lt;P&gt;I use kw36 board and sdk2.2.9 while using example as zipped in "AN12775SW.zip" download from nxp websit,which is an example about hrsotap, but after finish building, when doing debug, it give out "Thread #1 57005 (Suspended : Signal : SIGTRAP:Trace/breakpoint trap) 0xdeadbeee" ,which means&amp;nbsp;&lt;/P&gt;&lt;P&gt;Failed to execute MI command:&lt;BR /&gt;-data-disassemble -s 3735928558 -e 3735928698 -- 3&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Cannot access memory at address 0xdeadbeee&lt;/P&gt;&lt;P&gt;and according to "&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12775.pdf&amp;quot;" target="_blank" rel="noopener"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12775.pdf"&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I change to sdk2.2.2 ,it gives out the same error when debugging.&lt;/P&gt;&lt;P&gt;so I need your helps how to solve this.&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/168992"&gt;@EdgarLomeli&lt;/a&gt;&amp;nbsp;&amp;nbsp;@anyone who can give helps&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 01:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OTAP-about-hrs-by-example-on-KW36/m-p/1424853#M62577</guid>
      <dc:creator>yeyue</dc:creator>
      <dc:date>2022-03-09T01:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: OTAP about hrs by example on KW36</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OTAP-about-hrs-by-example-on-KW36/m-p/1425781#M62589</link>
      <description>&lt;P&gt;solved.because the bootloader has been modified by other man,so after change the bootloader back to "bootloader_otap_frdmkw36.bin",it works&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 03:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OTAP-about-hrs-by-example-on-KW36/m-p/1425781#M62589</guid>
      <dc:creator>yeyue</dc:creator>
      <dc:date>2022-03-10T03:34:47Z</dc:date>
    </item>
  </channel>
</rss>