<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K82 QSPI Individual Flash Mode B</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1420746#M62532</link>
    <description>&lt;P&gt;maybe this application note can help you&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5244.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5244.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Feb 2022 20:11:59 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2022-02-28T20:11:59Z</dc:date>
    <item>
      <title>K82 QSPI Individual Flash Mode B</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1420073#M62524</link>
      <description>&lt;P&gt;I have a board with a single flash device connected to the QuadSPI Bus Flash B. I'm using the FSL_QSPI driver. I have started from the qspi_polling example of the FRDM-K82F board and I have modified the flash configuration section in order to consider only the flash device on the B side:&lt;BR /&gt;&lt;BR /&gt;qspi_flash_config_t FlashConfig = {.flashA1Size = 0,&lt;BR /&gt;.flashA2Size = 0,&lt;BR /&gt;#if defined(FSL_FEATURE_QSPI_SUPPORT_PARALLEL_MODE) &amp;amp;&amp;amp; (FSL_FEATURE_QSPI_SUPPORT_PARALLEL_MODE)&lt;BR /&gt;.flashB1Size = FLASH_SIZE, /* 16MB */&lt;BR /&gt;.flashB2Size = 0,&lt;BR /&gt;#endif&lt;BR /&gt;#if !defined(FSL_FEATURE_QSPI_HAS_NO_TDH) || (!FSL_FEATURE_QSPI_HAS_NO_TDH)&lt;BR /&gt;.dataHoldTime = 0,&lt;BR /&gt;#endif&lt;BR /&gt;.CSHoldTime = 0,&lt;BR /&gt;.CSSetupTime = 0,&lt;BR /&gt;.cloumnspace = 0,&lt;BR /&gt;.dataLearnValue = 0,&lt;BR /&gt;.endian = kQSPI_64LittleEndian,&lt;BR /&gt;.enableWordAddress = false};&lt;BR /&gt;&lt;BR /&gt;The flash chip is an Infineon S25FL128SAGNFI01. The sector size is 256KB, while the page size is 512 bytes. I have also checked that the LUT command codes are the correct ones and any other associated parameter.&lt;BR /&gt;Unfortunately I can't read correctly the external flash memory. The read values are &lt;SPAN class=""&gt;inconsistent.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have read the RM thoroughly, but I can't find were I'm wrong. Could some expert help me finding the right way of using a single flash memory on qspi flash bus B side? Maybe there's something wrong with the memory mapping?&lt;BR /&gt;&lt;BR /&gt;Thank you very much in advance.&lt;/P&gt;&lt;H3&gt;&amp;nbsp;&lt;/H3&gt;</description>
      <pubDate>Sun, 27 Feb 2022 09:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1420073#M62524</guid>
      <dc:creator>TheRocketMan</dc:creator>
      <dc:date>2022-02-27T09:51:23Z</dc:date>
    </item>
    <item>
      <title>Re: K82 QSPI Individual Flash Mode B</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1420746#M62532</link>
      <description>&lt;P&gt;maybe this application note can help you&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5244.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5244.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Feb 2022 20:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1420746#M62532</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-02-28T20:11:59Z</dc:date>
    </item>
    <item>
      <title>Re: K82 QSPI Individual Flash Mode B</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1465426#M63179</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Did you found any soution to this problem?&lt;/P&gt;</description>
      <pubDate>Fri, 27 May 2022 08:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-QSPI-Individual-Flash-Mode-B/m-p/1465426#M63179</guid>
      <dc:creator>andreaswickstrom</dc:creator>
      <dc:date>2022-05-27T08:27:56Z</dc:date>
    </item>
  </channel>
</rss>