<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 MK60DN512 PTC5 Pin Features</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512-PTC5-Pin-Features/m-p/1408431#M62342</link>
    <description>&lt;P&gt;I've never used Kinetis mcu's before. Can I capture input with PTC5 pin of MK60DN controller? What is the resolution? Can I measure at 0.5ns resolution?&lt;BR /&gt;Note: I will use it to detect and measure a signal pulse that is 5 ns wide.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Feb 2022 06:59:28 GMT</pubDate>
    <dc:creator>burakgvl</dc:creator>
    <dc:date>2022-02-03T06:59:28Z</dc:date>
    <item>
      <title>MK60DN512 PTC5 Pin Features</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512-PTC5-Pin-Features/m-p/1408431#M62342</link>
      <description>&lt;P&gt;I've never used Kinetis mcu's before. Can I capture input with PTC5 pin of MK60DN controller? What is the resolution? Can I measure at 0.5ns resolution?&lt;BR /&gt;Note: I will use it to detect and measure a signal pulse that is 5 ns wide.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 06:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512-PTC5-Pin-Features/m-p/1408431#M62342</guid>
      <dc:creator>burakgvl</dc:creator>
      <dc:date>2022-02-03T06:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: MK60DN512 PTC5 Pin Features</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512-PTC5-Pin-Features/m-p/1410692#M62383</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196478"&gt;@burakgvl&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;No, you can't measure in 0.5ns resolution. Because 0.5ns need 2Ghz sample rate. But K60DN max speed is 150M. Timer hasn't such a high clock source.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 05:54:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512-PTC5-Pin-Features/m-p/1410692#M62383</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-02-09T05:54:46Z</dc:date>
    </item>
  </channel>
</rss>