<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックERR in using SWD_DIO pin to gpio pin</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERR-in-using-SWD-DIO-pin-to-gpio-pin/m-p/1405731#M62310</link>
    <description>&lt;P&gt;I want to use SWD_DIO pin to PTA4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but when i debug, if code go through this code, debugger shows me 'no source available for "__isr_vector() 0x4"'&lt;/P&gt;&lt;P&gt;and debug stops.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;why this problem happen? datasheet says SWD_DIO pin is 'Serial Wire Debug Data input/output', so debug process can't go more?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jan 2022 05:39:52 GMT</pubDate>
    <dc:creator>ETSZ</dc:creator>
    <dc:date>2022-01-27T05:39:52Z</dc:date>
    <item>
      <title>ERR in using SWD_DIO pin to gpio pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERR-in-using-SWD-DIO-pin-to-gpio-pin/m-p/1405731#M62310</link>
      <description>&lt;P&gt;I want to use SWD_DIO pin to PTA4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but when i debug, if code go through this code, debugger shows me 'no source available for "__isr_vector() 0x4"'&lt;/P&gt;&lt;P&gt;and debug stops.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;why this problem happen? datasheet says SWD_DIO pin is 'Serial Wire Debug Data input/output', so debug process can't go more?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 05:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERR-in-using-SWD-DIO-pin-to-gpio-pin/m-p/1405731#M62310</guid>
      <dc:creator>ETSZ</dc:creator>
      <dc:date>2022-01-27T05:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: ERR in using SWD_DIO pin to gpio pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERR-in-using-SWD-DIO-pin-to-gpio-pin/m-p/1405770#M62312</link>
      <description>&lt;P&gt;Yes, if you map a pin used by SWD/Debug as a GPIO pin, you won't be able to debug any more.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 06:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERR-in-using-SWD-DIO-pin-to-gpio-pin/m-p/1405770#M62312</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-01-27T06:39:03Z</dc:date>
    </item>
  </channel>
</rss>