<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Are the MK2 UART_RX pins 5V tolerant</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402141#M62279</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Pat,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience we bring you!&lt;BR /&gt;IO on MK26 are not 5V tolerant.&lt;BR /&gt;Part numbers that support 5V tolerant will be mentioned in the Data Sheet.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jan 2022 01:23:22 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-01-20T01:23:22Z</dc:date>
    <item>
      <title>Are the MK2 UART_RX pins 5V tolerant</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402018#M62276</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about the MK26FN2M0VMI18.&amp;nbsp; Are the UART_RX pins 5V tolerant?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have taken over a design from an engineer that has left our company.&amp;nbsp; And he has a 5V RS485 signal going to an UART_RX pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do not see in the datasheet that this pin is 5V tolerant.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 18:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402018#M62276</guid>
      <dc:creator>patrickirwin</dc:creator>
      <dc:date>2022-01-19T18:43:15Z</dc:date>
    </item>
    <item>
      <title>Re: Are the MK2 UART_RX pins 5V tolerant</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402141#M62279</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Pat,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience we bring you!&lt;BR /&gt;IO on MK26 are not 5V tolerant.&lt;BR /&gt;Part numbers that support 5V tolerant will be mentioned in the Data Sheet.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 01:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402141#M62279</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-01-20T01:23:22Z</dc:date>
    </item>
  </channel>
</rss>