<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I immediately start the user application written in the microcontroller? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-immediately-start-the-user-application-written-in-the/m-p/1398739#M62232</link>
    <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="スクリーンショット 2022-01-13 172432.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167522i60B2C1813F7D2A96/image-size/medium?v=v2&amp;amp;px=400" role="button" title="スクリーンショット 2022-01-13 172432.png" alt="スクリーンショット 2022-01-13 172432.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="スクリーンショット 2022-01-13 172809.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167523i3264E0A7BEFBFF57/image-size/medium?v=v2&amp;amp;px=400" role="button" title="スクリーンショット 2022-01-13 172809.png" alt="スクリーンショット 2022-01-13 172809.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Is there a way to start the user application written in the microcomputer immediately after turning on the power?&lt;BR /&gt;The MCU and Flash Tool I am using are as follows.&lt;/P&gt;&lt;P&gt;MCU : MKL43Z256VLH4&lt;BR /&gt;FlashTool : KinetisFlashTool&lt;/P&gt;&lt;P&gt;Also, I have already tried the following, but I haven't been able to start it immediately.&lt;/P&gt;&lt;P&gt;Start Kinetis Flash Tool&lt;BR /&gt;→ Select "BCA Utilities"&lt;BR /&gt;→ Select "Config"&lt;BR /&gt;→ Check "Tag", "Enable Direct Boot"&lt;BR /&gt;→ Select "OK"&lt;BR /&gt;→ Select "Save"&lt;BR /&gt;→ Update the firmware using Kinetis Flash Tool&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jan 2022 08:32:10 GMT</pubDate>
    <dc:creator>kyohei</dc:creator>
    <dc:date>2022-01-13T08:32:10Z</dc:date>
    <item>
      <title>How can I immediately start the user application written in the microcontroller?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-immediately-start-the-user-application-written-in-the/m-p/1398739#M62232</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="スクリーンショット 2022-01-13 172432.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167522i60B2C1813F7D2A96/image-size/medium?v=v2&amp;amp;px=400" role="button" title="スクリーンショット 2022-01-13 172432.png" alt="スクリーンショット 2022-01-13 172432.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="スクリーンショット 2022-01-13 172809.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167523i3264E0A7BEFBFF57/image-size/medium?v=v2&amp;amp;px=400" role="button" title="スクリーンショット 2022-01-13 172809.png" alt="スクリーンショット 2022-01-13 172809.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Is there a way to start the user application written in the microcomputer immediately after turning on the power?&lt;BR /&gt;The MCU and Flash Tool I am using are as follows.&lt;/P&gt;&lt;P&gt;MCU : MKL43Z256VLH4&lt;BR /&gt;FlashTool : KinetisFlashTool&lt;/P&gt;&lt;P&gt;Also, I have already tried the following, but I haven't been able to start it immediately.&lt;/P&gt;&lt;P&gt;Start Kinetis Flash Tool&lt;BR /&gt;→ Select "BCA Utilities"&lt;BR /&gt;→ Select "Config"&lt;BR /&gt;→ Check "Tag", "Enable Direct Boot"&lt;BR /&gt;→ Select "OK"&lt;BR /&gt;→ Select "Save"&lt;BR /&gt;→ Update the firmware using Kinetis Flash Tool&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 08:32:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-immediately-start-the-user-application-written-in-the/m-p/1398739#M62232</guid>
      <dc:creator>kyohei</dc:creator>
      <dc:date>2022-01-13T08:32:10Z</dc:date>
    </item>
    <item>
      <title>Re: How can I immediately start the user application written in the microcontroller?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-immediately-start-the-user-application-written-in-the/m-p/1400033#M62248</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195709"&gt;@kyohei&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;After downloading,&amp;nbsp;KinetisFlashTool will reset target. And the MCU will read FOPT and then, if execute ROM bootloader, it will read BCA. So, you can&lt;/P&gt;
&lt;P&gt;1. disable ROM bootloader by FOPT[BOOTSRC_SEL], or&lt;/P&gt;
&lt;P&gt;2. If you want to keep ROM bootloader, you can set a short timeout in BCA, or&lt;/P&gt;
&lt;P&gt;3. If you need a long timeout period, you have to use blhost.exe instead of KinetisFlashTool. Please refer to Table 13-2 in reference manual. ROM bootloader support 'Execute' command which can run user application code. But KinetisFlashTools doesn't support it. You can use blhost to download and execute.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 07:32:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-immediately-start-the-user-application-written-in-the/m-p/1400033#M62248</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-01-17T07:32:48Z</dc:date>
    </item>
  </channel>
</rss>