<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Flexbus and Parallel NOR FLASH connection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1396668#M62210</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191360"&gt;@NEIL4&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;You can refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-FlexBus-ALE/m-p/432605" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-FlexBus-ALE/m-p/432605&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Mon, 10 Jan 2022 09:19:55 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2022-01-10T09:19:55Z</dc:date>
    <item>
      <title>Flexbus and Parallel NOR FLASH connection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1396091#M62202</link>
      <description>&lt;P&gt;Im interfacing MK64FX Flexbus config as (16bit multiplexed) with Parallel NOR flash&amp;nbsp;SST39VF802C which is Word(16bit) &lt;EM&gt;programmed.(With Ref AN4393)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The Parallel NOR flash has Address lines(0-18).&lt;/P&gt;&lt;P&gt;Which type of latch should you recommend and what should be the hardware connection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 10:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1396091#M62202</guid>
      <dc:creator>NEIL4</dc:creator>
      <dc:date>2022-01-07T10:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus and Parallel NOR FLASH connection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1396668#M62210</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191360"&gt;@NEIL4&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;You can refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-FlexBus-ALE/m-p/432605" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-FlexBus-ALE/m-p/432605&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 09:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1396668#M62210</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-01-10T09:19:55Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus and Parallel NOR FLASH connection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1485305#M63518</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185748i3D2FF5CDB40BFE11/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have interfaced 16bit NOR flash(SST39LF802C) with MK64 via Latch (54ABT16373A), the connections are made as per the above diagram. Programming had done as per App. Note(AN4393).&lt;/P&gt;&lt;P&gt;During read, write and erase, the OE and R/W# are always at HIGH logic state. Due to which could not able to perform any operation on the flash. Any feedback is really helpful. Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 10:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-and-Parallel-NOR-FLASH-connection/m-p/1485305#M63518</guid>
      <dc:creator>NEIL4</dc:creator>
      <dc:date>2022-07-06T10:21:10Z</dc:date>
    </item>
  </channel>
</rss>