<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART DMA problem in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394275#M62173</link>
    <description>&lt;P&gt;This is my config function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;void DMA_Init(void)
{
    //enable clock for DMAMUX and DMA
    SIM_SCGC6 |= SIM_SCGC6_DMAMUX0_MASK;
    SIM_SCGC7 |= SIM_SCGC7_DMA_MASK;

    DMAMUX0_CHCFG0 = 0;

    //setup control and status register
    //should be inactive before write
    DMA_TCD0_CSR = 0;

    //enable request signal for channel 0
    DMA_ERQ = DMA_ERQ_ERQ0_MASK;

    //set memory address for source and destination
    DMA_TCD0_SADDR = (uint32_t)&amp;amp;log_buffer_data_1; //global scope buffer
    DMA_TCD0_DADDR = (uint32_t)&amp;amp;UART0_D;

    //set an offset
    //We increment the address by one, after each cycle
    DMA_TCD0_SOFF = 1;
    DMA_TCD0_DOFF = 0;

    //set data transfer size - 0 = byte
    DMA_TCD0_ATTR = DMA_ATTR_SSIZE(0) | DMA_ATTR_DSIZE(0);

    //number of bytes to be transfered in each service request
    DMA_TCD0_NBYTES_MLNO = glob_data_chank;

    //current major iteration count (a single iteration)
    //current major iteration count
    DMA_TCD0_CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(1);
    DMA_TCD0_BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(1);

    DMA_TCD0_SLAST = 0; 
    DMA_TCD0_DLASTSGA = 0; 

    //enable channel 0 and set the source - 3 = UART0 Transmit ($3.3.9.1 Table 3-26)
    DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(3);

    DMA_TCD0_CSR = DMA_CSR_DREQ_MASK | DMA_CSR_DONE_MASK;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it's kind of a dead end situation - until a first trigger&lt;/P&gt;&lt;P&gt;DMA_Start(buffer, size)&lt;/P&gt;&lt;P&gt;the DMA_CSR_DONE_MASK flag isn't set. On the other hand I can not start a transaction if I'm not sure the previous (or none) is complete.&lt;/P&gt;&lt;P&gt;Is there another way to know that DMA is ready for the next transaction? And how it should be handled properly ( if I may ask such an outrageous question)?&lt;/P&gt;</description>
    <pubDate>Tue, 04 Jan 2022 15:39:32 GMT</pubDate>
    <dc:creator>john71</dc:creator>
    <dc:date>2022-01-04T15:39:32Z</dc:date>
    <item>
      <title>UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1393672#M62152</link>
      <description>&lt;P&gt;I send a buffer&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;void DMA_Start(uint8_t *data, uint32_t pakage_size)
{
    while ((DMA_TCD0_CSR &amp;amp; DMA_CSR_DONE_MASK) == 0);

    //size to be transferred - reload each request
    DMA_TCD0_NBYTES_MLNO = pakage_size;

    //set memory address for source and destination 
    DMA_TCD0_SADDR = (uint32_t)&amp;amp;data;
    DMA_TCD0_DADDR = (uint32_t)&amp;amp;UART0_D;

    //current major iteration count
    DMA_TCD0_CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(1);
    //starting major iteration count
    DMA_TCD0_BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(1);

    //enable auto disable request feature
    DMA_TCD0_CSR |= DMA_CSR_DREQ_MASK;
    //enable major interrupt
    DMA_TCD0_CSR |= DMA_CSR_INTMAJOR_MASK;

    //enable request signal for channel 0
    DMA_ERQ = DMA_ERQ_ERQ0_MASK;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I call DMA_Start it seems like working, at least I don't get any exception. But I see no bytes coming out of TX pin.&lt;/P&gt;&lt;P&gt;How&amp;nbsp; can I be sure DMA is active and working?&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 06:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1393672#M62152</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2022-01-03T06:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1393775#M62162</link>
      <description>&lt;P&gt;The 'Done' flag must be cleared to configure the DMA.&lt;BR /&gt;This code is waiting for it to be set then never clearing it.&lt;BR /&gt;&lt;BR /&gt;Is the '|=' (OR assignment) appropriate for assigning to CSR?&lt;BR /&gt;&lt;BR /&gt;The order things are configured matter, check the reference manual.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 13:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1393775#M62162</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2022-01-03T13:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1393800#M62163</link>
      <description>&lt;P&gt;What better way to clear the flag?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;DMA_TCD0_CSR &amp;amp;= ~DMA_CSR_DONE_MASK;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Or&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;DMA_CDNE |= DMA_CDNE_CDNE(0);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About the '|=' (OR assignment) - I don't know.&lt;/P&gt;&lt;P&gt;The order things - so much as I could understand from the reference manual. Not sure my understanding is correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I clear DMA_CSR_DONE_MASK flag - it always stays in&lt;/P&gt;&lt;PRE&gt;while ((DMA_TCD0_CSR &amp;amp; DMA_CSR_DONE_MASK) == 0);&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 15:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1393800#M62163</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2022-01-03T15:33:35Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394261#M62170</link>
      <description>&lt;P&gt;Unless there is a good reason to carry set bits from one transaction to the next, simply clearing CSR works:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;DMA_TCD0_CSR = 0UL;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;If I clear DMA_CSR_DONE_MASK flag - it always stays in&lt;/P&gt;&lt;PRE&gt;while ((DMA_TCD0_CSR &amp;amp; DMA_CSR_DONE_MASK) == 0);&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Which is also indicating that something is not set correctly, being the transaction never starts so it won't ever be 'Done'.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jan 2022 13:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394261#M62170</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2022-01-04T13:19:36Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394275#M62173</link>
      <description>&lt;P&gt;This is my config function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;void DMA_Init(void)
{
    //enable clock for DMAMUX and DMA
    SIM_SCGC6 |= SIM_SCGC6_DMAMUX0_MASK;
    SIM_SCGC7 |= SIM_SCGC7_DMA_MASK;

    DMAMUX0_CHCFG0 = 0;

    //setup control and status register
    //should be inactive before write
    DMA_TCD0_CSR = 0;

    //enable request signal for channel 0
    DMA_ERQ = DMA_ERQ_ERQ0_MASK;

    //set memory address for source and destination
    DMA_TCD0_SADDR = (uint32_t)&amp;amp;log_buffer_data_1; //global scope buffer
    DMA_TCD0_DADDR = (uint32_t)&amp;amp;UART0_D;

    //set an offset
    //We increment the address by one, after each cycle
    DMA_TCD0_SOFF = 1;
    DMA_TCD0_DOFF = 0;

    //set data transfer size - 0 = byte
    DMA_TCD0_ATTR = DMA_ATTR_SSIZE(0) | DMA_ATTR_DSIZE(0);

    //number of bytes to be transfered in each service request
    DMA_TCD0_NBYTES_MLNO = glob_data_chank;

    //current major iteration count (a single iteration)
    //current major iteration count
    DMA_TCD0_CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(1);
    DMA_TCD0_BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(1);

    DMA_TCD0_SLAST = 0; 
    DMA_TCD0_DLASTSGA = 0; 

    //enable channel 0 and set the source - 3 = UART0 Transmit ($3.3.9.1 Table 3-26)
    DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(3);

    DMA_TCD0_CSR = DMA_CSR_DREQ_MASK | DMA_CSR_DONE_MASK;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it's kind of a dead end situation - until a first trigger&lt;/P&gt;&lt;P&gt;DMA_Start(buffer, size)&lt;/P&gt;&lt;P&gt;the DMA_CSR_DONE_MASK flag isn't set. On the other hand I can not start a transaction if I'm not sure the previous (or none) is complete.&lt;/P&gt;&lt;P&gt;Is there another way to know that DMA is ready for the next transaction? And how it should be handled properly ( if I may ask such an outrageous question)?&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jan 2022 15:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394275#M62173</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2022-01-04T15:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394333#M62175</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;1.&lt;/P&gt;&lt;PRE&gt;DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(3);&lt;/PRE&gt;&lt;P&gt;is suspect since it assumes the register is 0 (the OR should probably be removed).&lt;BR /&gt;&lt;BR /&gt;2. Also the UART needs to be configured to work with DMA, otherwise it won't trigger it.&lt;BR /&gt;&lt;BR /&gt;3. It is best to work with an end of transfer interrupt rather than blocking while waiting for it to complete (otherwise the processor is still running at full power, without doing anything else, apart from servicing interrupts)&lt;BR /&gt;&lt;BR /&gt;4. Compare with the methods in the open source uTasker project at &lt;A href="https://github.com/uTasker/uTasker-Kinetis" target="_blank" rel="noopener nofollow noreferrer"&gt;https://github.com/uTasker/uTasker-Kinetis&lt;/A&gt;&lt;BR /&gt;For example in kinetis_DMA.h the routine fnConfigDMA_buffer() is a general purpose buffer/buffer, buffer to peripheral, peripheral to buffer method which sets up all required details.&lt;BR /&gt;&lt;BR /&gt;You can also run the uTasker project as simulated Kinetis part in Visual studio and it will emulate the DMA / UART operation (making investigation, understanding and debugging simple) and report errors in the use of the DMA if it finds any.&lt;BR /&gt;All UARTs and LPUARTs support interrupt driven or DMA driven mode as standard.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 04 Jan 2022 16:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394333#M62175</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2022-01-04T16:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394631#M62180</link>
      <description>&lt;P&gt;Sorry, it's an old large complicated project. I can not port it to uTasker.&lt;/P&gt;&lt;P&gt;Actually in my case as I need to send in a loop a large amount of data no difference polling or interrupt - I have to wait previous transaction to complete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;while (datasize)
{
   //calculate the next chunk address
   //omitted 

  //double buffering
  //read chunk from NAND FLASH
   if (tog_buf)
	NFLASH_ReadPage(row_address, page_addr, log_buffer_data_1, page_chunk);	
    else
        NFLASH_ReadPage(row_address, page_addr, log_buffer_data_2, page_chunk);
	
    //does it matter?
    //while ((DMA_TCD0_CSR &amp;amp; DMA_CSR_DONE_MASK) == 0);    	
    while(interrupt_occur == 0);
        interrupt_occur = 0;

    //double buffering
     if (tog_buf)
        DMA_Start(log_buffer_data_1, page_chunk);
    else
    DMA_Start(log_buffer_data_2, page_chunk);

    offset += page_chunk;
    datasize -= page_chunk;

    tog_buf ^= 1;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A dead end situation - I wait for a&amp;nbsp; previous done flag but it never was triggered.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 08:27:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1394631#M62180</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2022-01-05T08:27:59Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1395189#M62188</link>
      <description>&lt;P&gt;Hi John&lt;BR /&gt;&lt;BR /&gt;I am not suggesting porting the project but instead using it as working reference. You can even put your code into its and use it simulator so see what happens and see why things don't operate if needed.&lt;BR /&gt;&lt;BR /&gt;For example this is the UART DMA initalisation:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;            uart_reg-&amp;gt;UART_C5 |= UART_C5_TDMAS;                          // use DMA rather than interrupts for transmission
            fnConfigDMA_buffer(UART_DMA_TX_CHANNEL[Channel], usDMAMUX, 0, 0, (void *)&amp;amp;(uart_reg-&amp;gt;UART_D), (DMA_BYTES | DMA_DIRECTION_OUTPUT | DMA_SINGLE_CYCLE), _uart_tx_dma_Interrupts[Channel], UART_DMA_TX_INT_PRIORITY[Channel]);
            uart_reg-&amp;gt;UART_C2 |= (UART_C2_TIE);                          // enable the tx dma request (DMA not yet enabled) rather than interrupt mode&lt;/LI-CODE&gt;&lt;P&gt;which may already be enough to identify what you are possibly missing [one clue it gives is that you need to enable &lt;U&gt;both&lt;/U&gt; DMA &lt;U&gt;and&lt;/U&gt; enable interrupts in the UART]. All DMA setup is in fnConfigDMA_buffer() (which works on any Kinetis DMA controller)&lt;BR /&gt;&lt;BR /&gt;This works on all Kinetis UARTs (any and all channels).&lt;BR /&gt;&lt;BR /&gt;To see how to start a transmission of a buffer content see fnTxByteDMA() which is, for the K10,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;// Start transfer of a block via DMA
//
extern QUEUE_TRANSFER fnTxByteDMA(QUEUE_HANDLE Channel, unsigned char *ptrStart, QUEUE_TRANSFER tx_length)
{
    KINETIS_DMA_TDC *ptrDMA_TCD = (KINETIS_DMA_TDC *)eDMA_DESCRIPTORS;
    ptrDMA_TCD += UART_DMA_TX_CHANNEL[Channel];
    ptrDMA_TCD-&amp;gt;DMA_TCD_BITER_ELINK = ptrDMA_TCD-&amp;gt;DMA_TCD_CITER_ELINK = tx_length; // the number of service requests (the number of bytes to be transferred)
    ptrDMA_TCD-&amp;gt;DMA_TCD_SADDR = (unsigned long)ptrStart;                 // source is tty output buffer's present location
    ATOMIC_PERIPHERAL_BIT_REF_SET(DMA_ERQ, UART_DMA_TX_CHANNEL[Channel]);// enable request source in order to start DMA activity
    return tx_length;
}&lt;/LI-CODE&gt;&lt;P&gt;Code is comprehensively commented/documented and is therefore very suitable for study/learning.&lt;BR /&gt;&lt;BR /&gt;The uTasker drivers adapt them selves to all Kinetis parts, with UARTs or LPUARTs, and whatever DMA controller the chip has and even run on i.MX RT parts [adapting itself just very slightly] (since the i.MX RT LPUARTs and DMA operation is compatible).&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 01:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1395189#M62188</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2022-01-06T01:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1395403#M62192</link>
      <description>&lt;P&gt;Sorry. I really fail to understand.&lt;/P&gt;&lt;P&gt;Should I include&amp;nbsp; kinetis_DMA.h in my project?&lt;/P&gt;&lt;P&gt;What does it mean - "use its simulator" ? What simulator? Where do I get it?&lt;/P&gt;&lt;P&gt;Where&lt;/P&gt;&lt;PRE&gt;fnTxByteDMA&lt;/PRE&gt;&lt;P&gt;is located?&lt;/P&gt;&lt;P&gt;Why&lt;/P&gt;&lt;P&gt;ptrDMA_TCD-&amp;gt;DMA_TCD_BITER_ELINK = ptrDMA_TCD-&amp;gt;DMA_TCD_CITER_ELINK = tx_length;&lt;/P&gt;&lt;P&gt;why not&lt;/P&gt;&lt;P&gt;ptrDMA_TCD-&amp;gt;DMA_TCD_BITER_ELINK = ptrDMA_TCD-&amp;gt;DMA_TCD_CITER_ELINK = 1;&lt;/P&gt;&lt;P&gt;it's major loop count - isn't it?&lt;/P&gt;&lt;P&gt;What should I learn from this -ptrDMA-&amp;gt;DMA_DCR |= (DMA_DCR_SINC); ? I don't have DMA_DCR&amp;nbsp; register. Where do I seek DMA_DCR_SINC define?&lt;/P&gt;&lt;P&gt;I just want to configure some registers right way and start a&amp;nbsp; DMA transfer.&lt;/P&gt;&lt;P&gt;And whet I'll have some free time I'd gladly learn uTasker.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 07:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1395403#M62192</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2022-01-06T07:22:16Z</dc:date>
    </item>
    <item>
      <title>Re: UART DMA problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1395497#M62195</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Tutorials (including simulation tutorial), documents and video guides for anything you don't understand:&lt;BR /&gt;&lt;A href="https://www.utasker.com/docs/documentation.html" target="_blank"&gt;https://www.utasker.com/docs/documentation.html&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.youtube.com/watch?v=kWNlsAoMly4&amp;amp;list=PLWKlVb_MqDQFZAulrUywU30v869JBYi9Q" target="_blank"&gt;https://www.youtube.com/watch?v=kWNlsAoMly4&amp;amp;list=PLWKlVb_MqDQFZAulrUywU30v869JBYi9Q&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I don't know that you want to actually use kinetis_DMA.h directly but you can copy some of its code if you need.&lt;/P&gt;&lt;P&gt;Simulator is in the project on Github.&lt;/P&gt;&lt;P&gt;fnTxByteDMA() is in the UART driver (kinetis_UART.h) and not in the DMA driver.&lt;/P&gt;&lt;P&gt;ptrDMA_TCD-&amp;gt;DMA_TCD_BITER_ELINK and ptrDMA_TCD-&amp;gt;DMA_TCD_CITER_ELINK are Starting Major Iteration Count and Current Major Iteration Count and can be set to the total number of bytes to be transferred. If you set to 1 the DMA will transfer one single byte and stop and need to be reconfigured and started again for each byte, which would make its use pointless in this particular instance. For UART transmission of a buffer it is the UART DMA request that kicks off each byte and the transfer performs the total count value before terminating.&lt;/P&gt;&lt;P&gt;DMA_DCR is in the DMA controller used by most of the KL parts (not K10, which has eDMA). You are looking at the wrong part of the code (see #if defined KINETIS_KL which is not relevant for your chip).&lt;/P&gt;&lt;P&gt;It is all C-code so you should be able to use it or copy its ideas to do the same things that you need to do; compare with your present code and maybe you will see what is missing or set incorrectly. The reference has been used in hundreds of industrial product designs since 2011 and so can be considered a proven efficient and reliable reference, so it makes sense to use it as reference/starting point for alternative implementations.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 08:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-problem/m-p/1395497#M62195</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2022-01-06T08:46:37Z</dc:date>
    </item>
  </channel>
</rss>