<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USBDM and MK20DN512ZVLL10 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-and-MK20DN512ZVLL10/m-p/1390794#M62124</link>
    <description>&lt;P&gt;Hello, i have a problem with communication between the MK20DN512ZVLL10 MCU and the USBDM debugger. When i click to "Detect Chip" in ARM Flash programmer tool, It looks like it communicates (even on oscilloscope it looks well), but after few seconds of detecting chip, communication is terminated with an error message.&amp;nbsp;I also found that the MCU is not on the list. Maybe it is not supported by USBDM? If this can be the case, is it possible to add it? I tried it on two boards with the same result so the MCU should be not damaged.&lt;/P&gt;&lt;P&gt;I will be happy for any suggestion.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thank you&lt;/P&gt;&lt;P&gt;Jakub&lt;/P&gt;</description>
    <pubDate>Wed, 22 Dec 2021 13:09:11 GMT</pubDate>
    <dc:creator>lskelectronics</dc:creator>
    <dc:date>2021-12-22T13:09:11Z</dc:date>
    <item>
      <title>USBDM and MK20DN512ZVLL10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-and-MK20DN512ZVLL10/m-p/1390794#M62124</link>
      <description>&lt;P&gt;Hello, i have a problem with communication between the MK20DN512ZVLL10 MCU and the USBDM debugger. When i click to "Detect Chip" in ARM Flash programmer tool, It looks like it communicates (even on oscilloscope it looks well), but after few seconds of detecting chip, communication is terminated with an error message.&amp;nbsp;I also found that the MCU is not on the list. Maybe it is not supported by USBDM? If this can be the case, is it possible to add it? I tried it on two boards with the same result so the MCU should be not damaged.&lt;/P&gt;&lt;P&gt;I will be happy for any suggestion.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thank you&lt;/P&gt;&lt;P&gt;Jakub&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 13:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-and-MK20DN512ZVLL10/m-p/1390794#M62124</guid>
      <dc:creator>lskelectronics</dc:creator>
      <dc:date>2021-12-22T13:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM and MK20DN512ZVLL10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-and-MK20DN512ZVLL10/m-p/1392377#M62141</link>
      <description>&lt;P&gt;The ARM Flash programmer tool seems support MK20DN512&lt;STRONG&gt;Z&lt;/STRONG&gt;VLL10.&lt;BR /&gt;Have you tried mass erase?&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Known Issues USBDM.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166320iA23F01F8FECA03AF/image-size/large?v=v2&amp;amp;px=999" role="button" title="Known Issues USBDM.png" alt="Known Issues USBDM.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Known Issues USBDM.png&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;About the waveform on reset_b, for blank new chip(after mass erase) it's normal phenomenon.&lt;BR clear="none" /&gt;If you flash a program for&amp;nbsp;MK20DN512VLL10 to&amp;nbsp;MK20DN512&lt;STRONG&gt;Z&lt;/STRONG&gt;VLL10, then hard fault will cause the reset too.&lt;BR clear="none" /&gt;If you have a debugger from &lt;A href="http://www.pemicro.com/" target="_self"&gt;PEMicro&lt;/A&gt;, you can halt the MCU by refer:&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2021/05/20/recovering-cortex-m-microcontroller-with-a-power-glitch/" target="_blank" rel="noopener" shape="rect"&gt;Recovering Cortex-M Microcontroller with a Power Glitch&amp;nbsp;&lt;/A&gt;&lt;BR clear="none" /&gt;If you have a debugger from Segger, you can refer:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-error-while-accessing-MDM-AP/m-p/651153" target="_blank" rel="noopener" shape="rect"&gt;Communication error while accessing MDM-AP.&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 02:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-and-MK20DN512ZVLL10/m-p/1392377#M62141</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-12-28T02:35:09Z</dc:date>
    </item>
  </channel>
</rss>