<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Relocation of exception vector table about KEA128</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Relocation-of-exception-vector-table-about-KEA128/m-p/1385440#M62055</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to refresh the&amp;nbsp;software with&amp;nbsp;custom protocol via CAN interface.&amp;nbsp;Once bootloader jumps to app, app&amp;nbsp;will relocate the exception vector table(SCB_VTOR) immediately. Will the reset interrupt vector also be changed? I see that changing the IVBR has no effect on the location of the reset vector(0xFFFFFC-0xFFFFFF) about S12Z device, that is,&amp;nbsp;bootloader and app share the reset handler.&amp;nbsp;In addition, if a reset occurs during app&amp;nbsp;operation, is&amp;nbsp;SCB_VTOR reset to 0?&amp;nbsp;What is the detailed process from the reset event to running the bootloader startup code?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;</description>
    <pubDate>Mon, 13 Dec 2021 07:37:03 GMT</pubDate>
    <dc:creator>jeffcharles</dc:creator>
    <dc:date>2021-12-13T07:37:03Z</dc:date>
    <item>
      <title>Relocation of exception vector table about KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Relocation-of-exception-vector-table-about-KEA128/m-p/1385440#M62055</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to refresh the&amp;nbsp;software with&amp;nbsp;custom protocol via CAN interface.&amp;nbsp;Once bootloader jumps to app, app&amp;nbsp;will relocate the exception vector table(SCB_VTOR) immediately. Will the reset interrupt vector also be changed? I see that changing the IVBR has no effect on the location of the reset vector(0xFFFFFC-0xFFFFFF) about S12Z device, that is,&amp;nbsp;bootloader and app share the reset handler.&amp;nbsp;In addition, if a reset occurs during app&amp;nbsp;operation, is&amp;nbsp;SCB_VTOR reset to 0?&amp;nbsp;What is the detailed process from the reset event to running the bootloader startup code?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 07:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Relocation-of-exception-vector-table-about-KEA128/m-p/1385440#M62055</guid>
      <dc:creator>jeffcharles</dc:creator>
      <dc:date>2021-12-13T07:37:03Z</dc:date>
    </item>
    <item>
      <title>Re: Relocation of exception vector table about KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Relocation-of-exception-vector-table-about-KEA128/m-p/1386628#M62077</link>
      <description>&lt;P&gt;The reset interrupt vector should also be changed. I believe this Application Note will be useful for your inquiry: &lt;A href="https://www.nxp.com/docs/en/application-note/AN2295.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN2295.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 17:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Relocation-of-exception-vector-table-about-KEA128/m-p/1386628#M62077</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2021-12-14T17:27:44Z</dc:date>
    </item>
  </channel>
</rss>