<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 PGA features on MK20DX256VLH7</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PGA-features-on-MK20DX256VLH7/m-p/1381729#M61992</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm have a couple of questions about the PGA on the MK20DX256VLH7.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. PGA Chop Feature&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;According to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=K20P64M72SF1RM" target="_self"&gt;Reference Manual&lt;/A&gt; section &lt;STRONG&gt;&lt;EM&gt;31.3.18 ADC PGA Register (ADCx_PGA)&lt;/EM&gt;&lt;/STRONG&gt; the chip doesn't have the &lt;STRONG&gt;&lt;EM&gt;PGAOFSM&lt;/EM&gt;&lt;/STRONG&gt; and &lt;STRONG&gt;&lt;EM&gt;PGACHPb&lt;/EM&gt;&lt;/STRONG&gt; fields.&lt;/P&gt;&lt;P&gt;There is a section &lt;STRONG&gt;&lt;EM&gt;6.6.1.4 16-bit ADC with PGA characteristics with Chop enabled&lt;/EM&gt;&lt;/STRONG&gt; in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/K20P64M72SF1.pdf" target="_self"&gt;Data Sheet.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Is this feature only available in some versions of this chip?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. Use of external reference with VrefOut&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The data sheet and reference manual indicate that it is possible to use an external reference applied to VrefOut with the internal reference disabled.&amp;nbsp; It is unclear to me what voltage restrictions apply to this external reference.&amp;nbsp; For example, is it possible to extend the PGA input compliance range by use of an external 3.0V reference?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 06 Dec 2021 07:20:35 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2021-12-06T07:20:35Z</dc:date>
    <item>
      <title>PGA features on MK20DX256VLH7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PGA-features-on-MK20DX256VLH7/m-p/1381729#M61992</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm have a couple of questions about the PGA on the MK20DX256VLH7.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. PGA Chop Feature&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;According to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=K20P64M72SF1RM" target="_self"&gt;Reference Manual&lt;/A&gt; section &lt;STRONG&gt;&lt;EM&gt;31.3.18 ADC PGA Register (ADCx_PGA)&lt;/EM&gt;&lt;/STRONG&gt; the chip doesn't have the &lt;STRONG&gt;&lt;EM&gt;PGAOFSM&lt;/EM&gt;&lt;/STRONG&gt; and &lt;STRONG&gt;&lt;EM&gt;PGACHPb&lt;/EM&gt;&lt;/STRONG&gt; fields.&lt;/P&gt;&lt;P&gt;There is a section &lt;STRONG&gt;&lt;EM&gt;6.6.1.4 16-bit ADC with PGA characteristics with Chop enabled&lt;/EM&gt;&lt;/STRONG&gt; in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/K20P64M72SF1.pdf" target="_self"&gt;Data Sheet.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Is this feature only available in some versions of this chip?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. Use of external reference with VrefOut&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The data sheet and reference manual indicate that it is possible to use an external reference applied to VrefOut with the internal reference disabled.&amp;nbsp; It is unclear to me what voltage restrictions apply to this external reference.&amp;nbsp; For example, is it possible to extend the PGA input compliance range by use of an external 3.0V reference?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 07:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PGA-features-on-MK20DX256VLH7/m-p/1381729#M61992</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2021-12-06T07:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: PGA features on MK20DX256VLH7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PGA-features-on-MK20DX256VLH7/m-p/1388315#M62094</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/10904"&gt;@pgo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Many thanks for your patience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hoping you are well, according the Chop Feature, effectively, this PGA Registers fields are only available in the K20P144M120SF3RM variant of the chip Kinetis K20 Series.&lt;/P&gt;
&lt;P&gt;Then, about your question regarding the external reference with VrefOut, this VREF can be used for a maximum of 1.2V using an external reference and having internal reference (VREFH and VREFL) disabled as you mentioned.&lt;BR /&gt;You can refer to this thread of our community where a similar question was done: &lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746574" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746574&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I am so glad to assist you if you have more questions.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards.&lt;/P&gt;
&lt;P&gt;Pablo Avalos.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 19:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PGA-features-on-MK20DX256VLH7/m-p/1388315#M62094</guid>
      <dc:creator>PabloAvalos</dc:creator>
      <dc:date>2021-12-16T19:19:10Z</dc:date>
    </item>
  </channel>
</rss>