<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 FRDM-K66F doesn't boot up after reset</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1377796#M61946</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Today I wanted to start working with my brand new FRDM-K66F, but since I use Win11 it wasn't that easy. To get it working i tried reset and the microcontroller was finally seen by the computer as BOOTLOADER. I've looked up this problem and found out that it can be solved by giving&amp;nbsp;0244_k20dx_bl_0x8000.bin to K66F. After that the board turned off and won't turn on back. Using K66 Micro USB port demo is working, but with OpenSDAv2.1 nothing is happening. Also tried connecting it to the PC with Ubuntu 20.04, the result is the same.&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;</description>
    <pubDate>Sat, 27 Nov 2021 20:25:14 GMT</pubDate>
    <dc:creator>AmIWho</dc:creator>
    <dc:date>2021-11-27T20:25:14Z</dc:date>
    <item>
      <title>FRDM-K66F doesn't boot up after reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1377796#M61946</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Today I wanted to start working with my brand new FRDM-K66F, but since I use Win11 it wasn't that easy. To get it working i tried reset and the microcontroller was finally seen by the computer as BOOTLOADER. I've looked up this problem and found out that it can be solved by giving&amp;nbsp;0244_k20dx_bl_0x8000.bin to K66F. After that the board turned off and won't turn on back. Using K66 Micro USB port demo is working, but with OpenSDAv2.1 nothing is happening. Also tried connecting it to the PC with Ubuntu 20.04, the result is the same.&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;</description>
      <pubDate>Sat, 27 Nov 2021 20:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1377796#M61946</guid>
      <dc:creator>AmIWho</dc:creator>
      <dc:date>2021-11-27T20:25:14Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F doesn't boot up after reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1377841#M61948</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The development board has two mcu, one is k66 and the other is k20. The k20 is used for debugging the k66. The program in k20 has two parts. One is bootloader and the other is debugging firmware. We use bootloader to update the debugging firmware. Hold the reset button and power on, you will see the disk like 'bootloader' or 'maintenance'. Drag the debugging firmware into the disk to finish updating the firmware. If the disk shows 'bootloader', the bootloader is the old version. You need to update it. Because the debug firmware needs the new bootloader. You need a external debugger(like Jlink)&amp;nbsp; to flash the&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;0244_k20dx_bl_0x8000.bin. Follow the attachment to update the bootloader.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Da&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Nov 2021 01:39:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1377841#M61948</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-11-29T01:39:21Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F doesn't boot up after reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1380789#M61978</link>
      <description>&lt;P&gt;That's exactly where the problem is. It doesn't boot up at all using OpenSDAv2.1 port. Not even demo is working. And of course, the computer doesn't see it at all,&amp;nbsp;regardless of whether the reset button is pressed or not.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Dec 2021 17:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1380789#M61978</guid>
      <dc:creator>AmIWho</dc:creator>
      <dc:date>2021-12-02T17:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F doesn't boot up after reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1380899#M61979</link>
      <description>&lt;P&gt;It means your bootlaoder may be broken. You need an external debugger to flash the bootloader.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 01:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-doesn-t-boot-up-after-reset/m-p/1380899#M61979</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-12-03T01:42:11Z</dc:date>
    </item>
  </channel>
</rss>