<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK22FX512AVLL12 bootloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLL12-bootloader/m-p/1355271#M61696</link>
    <description>&lt;P&gt;We were forced to port our hardware from MK22FN512VLL12 to&amp;nbsp;MK22FX512AVLL12, which is the most similar MCU to&amp;nbsp;MK22FN512VLL12 available.&lt;/P&gt;&lt;P&gt;We&amp;nbsp;use USB HID bootloader from NXP_Kinetis_Bootloader_2_0_0 package, it has a bootloader, that can run on&amp;nbsp;MK22FN512VLL12. We flash new firmware to our board using KinetisFlashTool.exe. My question is: is there the same bootloader that can run on&amp;nbsp;MK22FX512AVLL12? If negative, what bootloader is the most similar one to&amp;nbsp;MK22FN512VLL12's USB HID bootloader we used? What changes do we have to do to code (one is obvious - MK22FX512AVLL12 doesnt have 48MHz IRC, we have external crystal on our board)?&lt;/P&gt;</description>
    <pubDate>Wed, 13 Oct 2021 19:08:15 GMT</pubDate>
    <dc:creator>dusek_martin</dc:creator>
    <dc:date>2021-10-13T19:08:15Z</dc:date>
    <item>
      <title>MK22FX512AVLL12 bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLL12-bootloader/m-p/1355271#M61696</link>
      <description>&lt;P&gt;We were forced to port our hardware from MK22FN512VLL12 to&amp;nbsp;MK22FX512AVLL12, which is the most similar MCU to&amp;nbsp;MK22FN512VLL12 available.&lt;/P&gt;&lt;P&gt;We&amp;nbsp;use USB HID bootloader from NXP_Kinetis_Bootloader_2_0_0 package, it has a bootloader, that can run on&amp;nbsp;MK22FN512VLL12. We flash new firmware to our board using KinetisFlashTool.exe. My question is: is there the same bootloader that can run on&amp;nbsp;MK22FX512AVLL12? If negative, what bootloader is the most similar one to&amp;nbsp;MK22FN512VLL12's USB HID bootloader we used? What changes do we have to do to code (one is obvious - MK22FX512AVLL12 doesnt have 48MHz IRC, we have external crystal on our board)?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 19:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLL12-bootloader/m-p/1355271#M61696</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2021-10-13T19:08:15Z</dc:date>
    </item>
    <item>
      <title>Re: MK22FX512AVLL12 bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLL12-bootloader/m-p/1356379#M61710</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/140889"&gt;@dusek_martin&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;There isn't other bootloader witch can use on MK22FX512AVLL12 directly. K60D100M has same clock structure. But it's clock is 100M. You have to modify the code too.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 09:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLL12-bootloader/m-p/1356379#M61710</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-10-15T09:45:58Z</dc:date>
    </item>
  </channel>
</rss>