<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using I2C to read and write EEPROM in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/1349850#M61622</link>
    <description>&lt;P&gt;you don't read what you written onto the eeprom?&lt;BR /&gt;&lt;BR /&gt;have you correctly manage the "page" on the eeprom?&amp;nbsp;&lt;BR /&gt;are you incorrectly read/write the same location but on a wrong page?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 04 Oct 2021 04:10:29 GMT</pubDate>
    <dc:creator>D4Worker</dc:creator>
    <dc:date>2021-10-04T04:10:29Z</dc:date>
    <item>
      <title>Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854426#M51278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use the Kinetis SDK v2.3 with a TWR-K64F to read and write a 16kBit serial EEPROM (&lt;A href="https://www.mouser.com/datasheet/2/268/21703d-74886.pdf" rel="nofollow noopener noreferrer" target="_blank"&gt;Microchip 24LC16B&lt;/A&gt;). Specifically, I am using the i2c_polling_b2b_transfer_master example and have simply changed the 7-bit slave address to that of the EEPROM (in this case, 0x50, which is just the control code (0b1010, as specified in the datasheet), plus a page address of 000).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also specify&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;CODE&gt;uint8_t deviceAddress = 0x00U;&lt;/CODE&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise, I use the example code as-is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The semihosting console output from running this code is:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;PRE&gt;&lt;P&gt;I2C board2board polling example -- Master transfer.
Master will send data : 0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7 
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f 
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17 
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Receive sent data from slave :
0x1f 0x10 0x11 0x12 0x13 0x14 0x15 0x16 
0x17 0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 
0xff 0xff 0xff 0xff 0xff 0xff 0xff 0xff 
0xff 0xff 0xff 0xff 0xff 0xff 0xff 0xff&lt;/P&gt;&lt;P&gt;
Error occured in the transfer !&lt;/P&gt;&lt;P&gt;End of I2C example .&lt;/P&gt;&lt;/PRE&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I've tried to step through the code in debug mode, but it's very hard to tell where things are going wrong. Is there any documentation of the I2C API that demonstrates the state machine that is implemented?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 01:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854426#M51278</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2019-02-12T01:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854427#M51279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think your code writes a buffer of data and reads a buffer of data but doesn't control the EEPROM's internal address. That means that (assuming after a power cycle) it will write to the page address 0, 1, 2,3,..n and then read back from the address n+1, n+2, n+3 etc. which will not read back the data that has been written (and the compare will fail).&lt;/P&gt;&lt;P&gt;This means that &lt;SPAN style="text-decoration: underline;"&gt;you need to control the internal address pointer&lt;/SPAN&gt; (the first byte of the data sent when writing and also write it just before reading back again, as described in the EEPROM's data sheet).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The uTasker project includes support for the EEPROM that you are using (it also simulates it) and below is the reference code to write and read to/from page 3 (for example).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#define ADD_EEPROM_READ           (0xa1 + (3 &amp;lt;&amp;lt; 1))                     &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;// read address of EEPROM (page 3)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define ADD_EEPROM_WRITE          (0xa0 + (3 &amp;lt;&amp;lt; 1))                     &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;// write address of EEPROM (page 3)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define OUR_I2C_CHANNEL           0                                     &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;// use I2C 0&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; QUEUE_HANDLE I2CPortID &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; NO_ID_ALLOCATED&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                        &lt;SPAN class="comment token"&gt;// handle of I2C interface&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;// Open I2C interface to communicate with an EEPROM, RTC, etc.&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;fnConfigI2C_Interface&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
    I2CTABLE tI2CParameters&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    tI2CParameters&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;Channel &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; OUR_I2C_CHANNEL&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    tI2CParameters&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;usSpeed &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;100&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                                        &lt;SPAN class="comment token"&gt;// 100k&lt;/SPAN&gt;
    tI2CParameters&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;Rx_tx_sizes&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;TxQueueSize &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;64&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                         &lt;SPAN class="comment token"&gt;// transmit queue size&lt;/SPAN&gt;
    tI2CParameters&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;Rx_tx_sizes&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;RxQueueSize &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;64&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                         &lt;SPAN class="comment token"&gt;// receive queue size&lt;/SPAN&gt;
    tI2CParameters&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;Task_to_wake &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                                     &lt;SPAN class="comment token"&gt;// no wake on transmission&lt;/SPAN&gt;

    &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;fnOpen&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;TYPE_I2C&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; FOR_I_O&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;tI2CParameters&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; NO_ID_ALLOCATED&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// open the channel with defined configurations&lt;/SPAN&gt;
        &lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; ucSetEEPROMAddress0&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;ADD_EEPROM_WRITE&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// command to set address to read to 0&lt;/SPAN&gt;
        &lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; ucReadEEPROM&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;16&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; ADD_EEPROM_READ&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; OWN_TASK&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// command to start a read of 16 bytes with the task scheduled when the read has completed&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;fnWrite&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;ucSetEEPROMAddress0&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ucSetEEPROMAddress0&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// write the EEPROM address to read&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;fnRead&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;ucReadEEPROM&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;             &lt;SPAN class="comment token"&gt;// start the read process of 16 bytes&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

Reception handler

&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;fnMsgs&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;                                        &lt;SPAN class="comment token"&gt;// if I2C message waiting&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;Length &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;fnRead&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; ucInputMessage&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; MEDIUM_MESSAGE&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        &lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; ucSetWriteEEPROM1&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;ADD_EEPROM_WRITE&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;3&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// prepare write of one byte to address 3&lt;/SPAN&gt;
        &lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; ucSetWriteEEPROM2&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;ADD_EEPROM_WRITE&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;3&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;6&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;9&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;10&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// prepare write of multiple bytes to address 5&lt;/SPAN&gt;
        &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; x &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;x &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt; Length&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;                                         &lt;SPAN class="comment token"&gt;// display received bytes&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;fnDebugHex&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ucInputMessage&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;x&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WITH_LEADIN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; WITH_SPACE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;fnDebugMsg&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"\r\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        &lt;SPAN class="comment token"&gt;// Now change the contents using two writes&lt;/SPAN&gt;
        &lt;SPAN class="comment token"&gt;//&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;fnWrite&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;ucSetWriteEEPROM1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ucSetWriteEEPROM1&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// start single byte write&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;fnWrite&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;I2CPortID&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;ucSetWriteEEPROM2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ucSetWriteEEPROM2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// start page write&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;On first use it reads and display the first 16 bytes in the page, then write 0x05 to address 3, followed by 3,4,5,..0xa to a addresses 5..12.&lt;/P&gt;&lt;P&gt;After a power cycle the values written (to verify they are non-volatile) are shown to be there as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/71945i9F08DFE2D0D40FAF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A binary file to do this on the FRDM-K64F is attached, whereby the I2C connections are on PTE24 and PTE25 and the debug interface on OpenSDA COM at 115200Baud.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/71979i6221D57A51A25B4B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Complete K64 solutions, training and support: &lt;A href="http://www.utasker.com/kinetis.html" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Kinetis K64:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/FRDM-K64F.html" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/kinetis/FRDM-K64F.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/TWR-K64F120M.html" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/kinetis/TWR-K64F120M.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/TEENSY_3.5.html" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/kinetis/TEENSY_3.5.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/Hexiwear-K64F.html" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/kinetis/Hexiwear-K64F.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I2C: &lt;A href="http://www.utasker.com/docs/uTasker/uTasker_I2C.pdf" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/docs/uTasker/uTasker_I2C.pdf&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854427#M51279</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-11-02T14:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854428#M51280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think it's the case that I am not controlling the internal address pointer of the EEPROM. The API function I2C_MasterTransferBlocking takes a pointer to the data type &lt;EM&gt;i2c_master_transfer_t&lt;/EM&gt;, which includes the slave address, subaddress, and subaddressSize as its members. (Annoyingly, the documentation for what subaddress and subaddressSize mean is completely missing, but I believe&amp;nbsp;that subaddress&amp;nbsp;is the first&amp;nbsp;8-bit register&amp;nbsp;you wish to access and subaddressSize is the size &lt;STRONG&gt;in bytes&lt;/STRONG&gt; of each register of the slave).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I can tell, the&amp;nbsp;&lt;SPAN&gt;I2C_MasterTransferBlocking proceeds as follows (for a read operation):&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. After some initial setup and status checks, I2C_MasterStart is called to initiate a transfer. This is responsible for sending the start signal, followed by the 7-bit slave address, plus the R/W bit.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Following some error checking, the subaddress is sent. I believe this is what the EEPROM data sheet considers the "Word Address."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3. For a read operation, a repeated START signal is sent. This should initiate the "Sequential Read" mode starting from the Word Address of step (2).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4. I2C_MasterReadBlocking is then called, reading in each byte until the rxSize counter indicates that only one byte is remaining, after which the master sends a NACK to stop the read operation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I altered the i2c_polling_b2b_transfer_master.c code to perform an initial read of the EEPROM, followed by a write, and finally a second read. This indicates that the internal address pointer for the EEPROM is being controlled, because the the initial and final read operations output the same data (i.e., the address pointer is not simply incrementing from 0,1,2,...n-1, then from n, n+1,...2*n-1, and finally from 2n, 2n+1,...3n-1, for the read, write, and read operations respectively).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response, but I would prefer to avoid adding the complication of uTasker to my current project as it's already pretty far along. It would be much more helpful to understand where the I2C communication between the K64 and the EEPROM is going wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 17:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854428#M51280</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2019-02-12T17:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854429#M51281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Andy&lt;BR /&gt;&lt;BR /&gt;I don't know the API that you are using but had the impression that it wasn't addressing correctly, but it may be a different problem (a driver bug or incorrect use of the API) so you will need to debug and best use a logic analyser to see what is on the bus (to avoid guess work).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 20:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854429#M51281</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-02-12T20:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854430#M51282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to sort this out. There were two issues:&lt;/P&gt;&lt;P&gt;1. The EEPROM that I am using has only a 16-byte page memory. If you try to write more than 16 bytes in a row (without sending a STOP) condition,&amp;nbsp;the data will wrap around and start overwriting at the start of the page. To fix this, I simply changed&amp;nbsp;&lt;BR /&gt;&lt;CODE&gt;#define I2C_DATA_LENGTH 33U&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;#define I2C_DATA_LENGTH 10U&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;2. The&amp;nbsp;example code from the SDK was also sending out the data length (originally,&amp;nbsp;"32") as the first transmitted byte. But the comparison between master and slave data was ignoring this 0th element (I don't know why), so the data stored in the EEPROM were all shifted by one register. To fix this, I simply deleted the line&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;g_master_txBuff[0] = I2C_DATA_LENGTH - 1U;&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;and instead fill the txBuff using a FOR loop with index starting from element zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So in summary, there is no issue with the API provided by SDK 2.3.0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 01:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/854430#M51282</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2019-02-14T01:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/1282197#M60617</link>
      <description>&lt;P&gt;I was also having this same problem, my solution was that when sending the memory address to be read to the slave, the length would be 2 bytes. I made this change and my problem was resolved.&lt;/P&gt;&lt;P&gt;follow the example ..&lt;BR /&gt;I just changed that data from:&lt;BR /&gt;masterXfer.subaddressSize = 1;&lt;/P&gt;&lt;P&gt;for:&lt;BR /&gt;masterXfer.subaddressSize = 2; // address in 2 bytes&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 03:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/1282197#M60617</guid>
      <dc:creator>RosimarSilva</dc:creator>
      <dc:date>2021-05-26T03:00:34Z</dc:date>
    </item>
    <item>
      <title>Re: Using I2C to read and write EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/1349850#M61622</link>
      <description>&lt;P&gt;you don't read what you written onto the eeprom?&lt;BR /&gt;&lt;BR /&gt;have you correctly manage the "page" on the eeprom?&amp;nbsp;&lt;BR /&gt;are you incorrectly read/write the same location but on a wrong page?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Oct 2021 04:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-I2C-to-read-and-write-EEPROM/m-p/1349850#M61622</guid>
      <dc:creator>D4Worker</dc:creator>
      <dc:date>2021-10-04T04:10:29Z</dc:date>
    </item>
  </channel>
</rss>