<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: ADC+DMA+SPI for FRDM-KV31F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-SPI-for-FRDM-KV31F/m-p/1347874#M61585</link>
    <description>&lt;P&gt;Hello Ray,&lt;/P&gt;
&lt;P&gt;The KV31 does have two ADCs which are capable of up to 1.2MSamples/second in 12bit mode. You mentioned 1Mbps, so it should be doable albeit it would also depend on the size of the samples.&lt;/P&gt;
&lt;P&gt;There is not an SDK example with exactly this configuration, but there are some ADC and SPI examples on the FRDM-KV31F SDK which may help as a starting point.&lt;/P&gt;
&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
    <pubDate>Tue, 28 Sep 2021 23:10:22 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2021-09-28T23:10:22Z</dc:date>
    <item>
      <title>ADC+DMA+SPI for FRDM-KV31F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-SPI-for-FRDM-KV31F/m-p/1346278#M61561</link>
      <description>&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; We need 2 channels 1Mbps ADC conversion rate to output result via SPI, is there any example source code for this in FRDM-KV31F?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Ray&lt;/P&gt;</description>
      <pubDate>Sun, 26 Sep 2021 08:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-SPI-for-FRDM-KV31F/m-p/1346278#M61561</guid>
      <dc:creator>ray_deng1</dc:creator>
      <dc:date>2021-09-26T08:56:45Z</dc:date>
    </item>
    <item>
      <title>Re: ADC+DMA+SPI for FRDM-KV31F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-SPI-for-FRDM-KV31F/m-p/1347874#M61585</link>
      <description>&lt;P&gt;Hello Ray,&lt;/P&gt;
&lt;P&gt;The KV31 does have two ADCs which are capable of up to 1.2MSamples/second in 12bit mode. You mentioned 1Mbps, so it should be doable albeit it would also depend on the size of the samples.&lt;/P&gt;
&lt;P&gt;There is not an SDK example with exactly this configuration, but there are some ADC and SPI examples on the FRDM-KV31F SDK which may help as a starting point.&lt;/P&gt;
&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 23:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-SPI-for-FRDM-KV31F/m-p/1347874#M61585</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-09-28T23:10:22Z</dc:date>
    </item>
  </channel>
</rss>