<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MKE02Z32VLC4 - ADC reference voltage range in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z32VLC4-ADC-reference-voltage-range/m-p/1343288#M61516</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i have a question about the microcontroller MKE02Z32VLC4.&lt;BR /&gt;Regarding to the Datasheet, the Voltage for V-DDA shall be between (VDD – 0.3V) and (VDD + 0.3V).&lt;BR /&gt;V-REFH is then on the same potential since its on the same pin (for QFN 32 package).&lt;/P&gt;&lt;P&gt;It looks like there is no option to power the controller with any voltage arround 5V, and use a external ADC&lt;BR /&gt;reference with +3.0V (for example).&lt;BR /&gt;Am i right with that assumtion, or have i missed something?&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 13:20:10 GMT</pubDate>
    <dc:creator>____</dc:creator>
    <dc:date>2021-09-21T13:20:10Z</dc:date>
    <item>
      <title>MKE02Z32VLC4 - ADC reference voltage range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z32VLC4-ADC-reference-voltage-range/m-p/1343288#M61516</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i have a question about the microcontroller MKE02Z32VLC4.&lt;BR /&gt;Regarding to the Datasheet, the Voltage for V-DDA shall be between (VDD – 0.3V) and (VDD + 0.3V).&lt;BR /&gt;V-REFH is then on the same potential since its on the same pin (for QFN 32 package).&lt;/P&gt;&lt;P&gt;It looks like there is no option to power the controller with any voltage arround 5V, and use a external ADC&lt;BR /&gt;reference with +3.0V (for example).&lt;BR /&gt;Am i right with that assumtion, or have i missed something?&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 13:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z32VLC4-ADC-reference-voltage-range/m-p/1343288#M61516</guid>
      <dc:creator>____</dc:creator>
      <dc:date>2021-09-21T13:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: MKE02Z32VLC4 - ADC reference voltage range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z32VLC4-ADC-reference-voltage-range/m-p/1343449#M61523</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191561"&gt;@____&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&amp;nbsp; If you power the MCU with VDD of 5V,&amp;nbsp; the VDDA&amp;nbsp; (analog supply)&amp;nbsp; should be in the&amp;nbsp; (5.0&lt;SPAN&gt;– 0.3&lt;/SPAN&gt;)v&amp;nbsp; and&amp;nbsp; (5.0 +&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;0.3&lt;/SPAN&gt;)v&amp;nbsp; &amp;nbsp;range.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The external reference pins&amp;nbsp;VREFL and&amp;nbsp;VREFH, should also follow VDDA and VSSA,&amp;nbsp; So, if VDDA is 5V,&amp;nbsp; the external VREFH should be at 5V too. And this is also restrictive because VREFH and VDDA are internally connected.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_1-1632250214765.png" style="width: 597px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/156627iD2D5FA4304F0FA33/image-dimensions/597x191?v=v2" width="597" height="191" role="button" title="diego_charles_1-1632250214765.png" alt="diego_charles_1-1632250214765.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;diego_charles_1-1632250214765.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So , as you point out :&lt;EM&gt; there is no option to power the controller with any voltage around&amp;nbsp;5V, and use a external ADC&amp;nbsp;reference with +3.0V&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;For design reference you could&amp;nbsp; check the&amp;nbsp; FRDM-KE02Z40M schematics.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;All the best,&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 19:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z32VLC4-ADC-reference-voltage-range/m-p/1343449#M61523</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2021-09-21T19:00:38Z</dc:date>
    </item>
  </channel>
</rss>