<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK66FN2M0VMD18 digital 5v input tolerant in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343041#M61509</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have used the&amp;nbsp; &lt;SPAN class="fontstyle0"&gt;MK61FN1M0VMD12&lt;/SPAN&gt;&amp;nbsp; part in the past and its spec said very clearly that all digital IO pins are 5V input tolerant.&amp;nbsp; see attachment for MK61 snap shot.&lt;/P&gt;&lt;P&gt;now, we are looking at&amp;nbsp;MK66FN2M0VMD18 device but can not find any 5v input tolerant on the data sheet.&amp;nbsp; we are surprised because the MK61F and MK66F should be the same family.&lt;/P&gt;&lt;P&gt;can you please clarify?&amp;nbsp; This is very confusing on why the same family part does not have the same 5v input tolerant.&lt;/P&gt;&lt;P&gt;Thanks and Best Regards,&lt;/P&gt;&lt;P&gt;Henry Nguyen&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 05:33:16 GMT</pubDate>
    <dc:creator>henrynguyen</dc:creator>
    <dc:date>2021-09-21T05:33:16Z</dc:date>
    <item>
      <title>MK66FN2M0VMD18 digital 5v input tolerant</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343041#M61509</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have used the&amp;nbsp; &lt;SPAN class="fontstyle0"&gt;MK61FN1M0VMD12&lt;/SPAN&gt;&amp;nbsp; part in the past and its spec said very clearly that all digital IO pins are 5V input tolerant.&amp;nbsp; see attachment for MK61 snap shot.&lt;/P&gt;&lt;P&gt;now, we are looking at&amp;nbsp;MK66FN2M0VMD18 device but can not find any 5v input tolerant on the data sheet.&amp;nbsp; we are surprised because the MK61F and MK66F should be the same family.&lt;/P&gt;&lt;P&gt;can you please clarify?&amp;nbsp; This is very confusing on why the same family part does not have the same 5v input tolerant.&lt;/P&gt;&lt;P&gt;Thanks and Best Regards,&lt;/P&gt;&lt;P&gt;Henry Nguyen&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 05:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343041#M61509</guid>
      <dc:creator>henrynguyen</dc:creator>
      <dc:date>2021-09-21T05:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: MK66FN2M0VMD18 digital 5v input tolerant</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343300#M61518</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/128384"&gt;@henrynguyen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What you're showing is exactly right, all the Kinetis pins, with the exception of the specified ones, in &lt;STRONG&gt;input mode&lt;/STRONG&gt; are 5V tolerant.&amp;nbsp; I recommend a 1k resistor between the 5V output to the Kinetis input pin to minimize any potential current flow from the output into the Kinetis.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We had a discussion on using the pins as Open Collector outputs and you can see it here:&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1302583" target="_blank" rel="noopener"&gt;5v Tolerant pins as Open Collector Drivers&lt;/A&gt;).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good luck!&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 13:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343300#M61518</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-09-21T13:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: MK66FN2M0VMD18 digital 5v input tolerant</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343312#M61519</link>
      <description>&lt;P&gt;Hi Myke_predko&lt;/P&gt;&lt;P&gt;thank you so much for your input. &amp;nbsp;&lt;BR /&gt;However I am still uneasy because I am not sure why NXP did not spell this out explicitly for K66F data sheet. &amp;nbsp;&lt;BR /&gt;In our application, the RXD pin from CAN transceiver drives a digital 5v to the K66F input. &amp;nbsp;The current is low but it is 5v and the K66F VDD is 3.3v. &amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;can someone from NXP please confirm if our assumptions are right and the data sheet will be updated to reflect this?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Henry&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 13:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1343312#M61519</guid>
      <dc:creator>henrynguyen</dc:creator>
      <dc:date>2021-09-21T13:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: MK66FN2M0VMD18 digital 5v input tolerant</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1347840#M61584</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/128384"&gt;@henrynguyen&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;The assumptions are correct all the Kinetis pins, with exception of the specified have an input mode of 5V tolerant.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;We will review out documentation in order to updated.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 20:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VMD18-digital-5v-input-tolerant/m-p/1347840#M61584</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2021-09-28T20:42:01Z</dc:date>
    </item>
  </channel>
</rss>