<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: How do I determine in code which micro is being used</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1340956#M61490</link>
    <description>&lt;P&gt;Hi&amp;nbsp;larrydemuth,&lt;/P&gt;
&lt;P&gt;You can check the value of&amp;nbsp;System Device Identification Register (SIM_SDID).&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 16 Sep 2021 00:35:11 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2021-09-16T00:35:11Z</dc:date>
    <item>
      <title>How do I determine in code which micro is being used</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1340856#M61488</link>
      <description>&lt;P&gt;With the disaster with getting NXP (and others) micros, I'm looking into switching to one that is available. But in my code I need to be able to tell which one I'm using.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a register or set of registers that would tell me if I'm using a MK66FN2M, or other micro?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 20:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1340856#M61488</guid>
      <dc:creator>larrydemuth</dc:creator>
      <dc:date>2021-09-15T20:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: How do I determine in code which micro is being used</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1340956#M61490</link>
      <description>&lt;P&gt;Hi&amp;nbsp;larrydemuth,&lt;/P&gt;
&lt;P&gt;You can check the value of&amp;nbsp;System Device Identification Register (SIM_SDID).&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 00:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1340956#M61490</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-09-16T00:35:11Z</dc:date>
    </item>
    <item>
      <title>Re: How do I determine in code which micro is being used</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1341587#M61500</link>
      <description>&lt;P&gt;Thats what I was looking for! Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 12:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-determine-in-code-which-micro-is-being-used/m-p/1341587#M61500</guid>
      <dc:creator>larrydemuth</dc:creator>
      <dc:date>2021-09-16T12:47:31Z</dc:date>
    </item>
  </channel>
</rss>