<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic what's the link between LCD waveform registers and LPUART. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-s-the-link-between-LCD-waveform-registers-and-LPUART/m-p/1327236#M61313</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on&amp;nbsp;MKM34Z256xxx7, it is connected to 32pin segment LCD and LPUART for communication purpose(both are working fine).&lt;/P&gt;&lt;P&gt;I run the controller in VLPR and VLPS modes by switching for every 1 second. I'm using LCD on PORTA, PORTB, PORTC, PORTD and LPUART on PORTI. The issue is, if I turn on all LCD segments by will filling (0xFF) in respective waveform registers and try to send some data on LPUART, I could able to receive only a few bytes on interrupt, not getting interrupt for rest of other bytes. The LPUART interrupts are not working. If I turn off a any single segment by writing (0x00) on LCD waveform registers, then my data goes normally on LPUART.&lt;/P&gt;&lt;P&gt;I verified clock initializations, interrupt enable/disable stuff, respective voltages on LPUART rx/tx pins, waveforms and controller switch to VLPR whenever it get tx/rx/edge interrupts&amp;nbsp; as well. I also found that if I keeps running in VLPR state, then everything working fine as expected. I was been working on this from past 3 days.&lt;/P&gt;&lt;P&gt;Please help me to crack this strange issue I'm facing. Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Avinash.&lt;/P&gt;</description>
    <pubDate>Sun, 22 Aug 2021 15:05:09 GMT</pubDate>
    <dc:creator>Avinash_7</dc:creator>
    <dc:date>2021-08-22T15:05:09Z</dc:date>
    <item>
      <title>what's the link between LCD waveform registers and LPUART.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-s-the-link-between-LCD-waveform-registers-and-LPUART/m-p/1327236#M61313</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on&amp;nbsp;MKM34Z256xxx7, it is connected to 32pin segment LCD and LPUART for communication purpose(both are working fine).&lt;/P&gt;&lt;P&gt;I run the controller in VLPR and VLPS modes by switching for every 1 second. I'm using LCD on PORTA, PORTB, PORTC, PORTD and LPUART on PORTI. The issue is, if I turn on all LCD segments by will filling (0xFF) in respective waveform registers and try to send some data on LPUART, I could able to receive only a few bytes on interrupt, not getting interrupt for rest of other bytes. The LPUART interrupts are not working. If I turn off a any single segment by writing (0x00) on LCD waveform registers, then my data goes normally on LPUART.&lt;/P&gt;&lt;P&gt;I verified clock initializations, interrupt enable/disable stuff, respective voltages on LPUART rx/tx pins, waveforms and controller switch to VLPR whenever it get tx/rx/edge interrupts&amp;nbsp; as well. I also found that if I keeps running in VLPR state, then everything working fine as expected. I was been working on this from past 3 days.&lt;/P&gt;&lt;P&gt;Please help me to crack this strange issue I'm facing. Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Avinash.&lt;/P&gt;</description>
      <pubDate>Sun, 22 Aug 2021 15:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-s-the-link-between-LCD-waveform-registers-and-LPUART/m-p/1327236#M61313</guid>
      <dc:creator>Avinash_7</dc:creator>
      <dc:date>2021-08-22T15:05:09Z</dc:date>
    </item>
    <item>
      <title>Re: what's the link between LCD waveform registers and LPUART.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-s-the-link-between-LCD-waveform-registers-and-LPUART/m-p/1330930#M61357</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190494"&gt;@Avinash_7&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;How is the problem going? Please check the NVIC-&amp;gt;IPCR register to see if the interrupt is pending and check NVIC-&amp;gt;ISER register to see if LPUART interrupt is enabled at that time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 08:50:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-s-the-link-between-LCD-waveform-registers-and-LPUART/m-p/1330930#M61357</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-08-27T08:50:19Z</dc:date>
    </item>
  </channel>
</rss>