<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB regulator no 3.3v comes out from VOUT33</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243388#M6130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the USB regulator is broken on the older two boards. Now I just solder a new board and add a 500ohm resistor between 5v and VREGIN. Then I measured the voltage output from VOUT33, it is 3.3v. The only differences is I add a 500ohm resistor between 5v and VREGIN. &lt;/P&gt;&lt;P&gt;I don't know if it is the reason causing the USB regulator damaged. But it seems it is very easy to break it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Dec 2013 19:49:47 GMT</pubDate>
    <dc:creator>danielchai</dc:creator>
    <dc:date>2013-12-05T19:49:47Z</dc:date>
    <item>
      <title>USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243383#M6125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am testing the USB device function on our board which uses MK60FN1M0VLQ12.&lt;/P&gt;&lt;P&gt;The connection is &lt;/P&gt;&lt;P&gt;USB 2.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCU(has independent power supply)&lt;/P&gt;&lt;P&gt;VCC------------------ VREGIN&lt;/P&gt;&lt;P&gt;D+&amp;nbsp; ------------------&amp;nbsp; USB0_DP&lt;/P&gt;&lt;P&gt;D-&amp;nbsp;&amp;nbsp; ------------------- USB0_DM&lt;/P&gt;&lt;P&gt;GND ----------------&amp;nbsp; GND&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VOUT33(floating)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I measure the VREGIN, it is 5v. But when I measure the VOUT33, it is about 0.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas about this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 18:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243383#M6125</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-12-04T18:45:01Z</dc:date>
    </item>
    <item>
      <title>Re: USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243384#M6126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible the USB regulator was damaged on that device?&amp;nbsp; Is this issue happening on more than one board?&amp;nbsp; The USB signals are exposed to transients, and should be properly protected.&amp;nbsp; Transients on the VREGIN in pin can damage the USB regulator.&amp;nbsp; Here are some other links discussing that issue, and some protection options for the USB signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/325183"&gt;Taking the Kinetis L FRDM board to the next level, a real product&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/305444"&gt;Re: Burnt two MK60FN1M0VLQ12 when plug in USB port&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 21:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243384#M6126</guid>
      <dc:creator>dereksnell</dc:creator>
      <dc:date>2013-12-04T21:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243385#M6127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure.&lt;/P&gt;&lt;P&gt;I tested it on tow boards.&lt;/P&gt;&lt;P&gt;On the first board, after I connect the 5V to VREGIN, I measure the voltage on the VREGIN pin, it is 0.3v to 0.5v. It seems on this board, the USB regulator is damaged.&amp;nbsp; &lt;/P&gt;&lt;P&gt;On the second board, after I connect the 5v to VREGIN, I measured the voltage on the VREGIN, it is 4.98v, but the VOUT33 is about 0.1v. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to make another board and add the protection circuit and check if it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 22:08:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243385#M6127</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-12-04T22:08:01Z</dc:date>
    </item>
    <item>
      <title>Re: USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243386#M6128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi, Daniel&lt;/P&gt;&lt;P&gt;Do you add bypass capacitor(about 0.1uF) to pin VOUT33? If not,please add then continue your testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 22:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243386#M6128</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-12-04T22:34:44Z</dc:date>
    </item>
    <item>
      <title>Re: USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243387#M6129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I added a capacitor to the pin VOUT33, but the output is still 0.1v.&lt;/P&gt;&lt;P&gt;Is there any way that I can check to make sure the USB regulator is broken?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2013 19:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243387#M6129</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-12-05T19:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243388#M6130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the USB regulator is broken on the older two boards. Now I just solder a new board and add a 500ohm resistor between 5v and VREGIN. Then I measured the voltage output from VOUT33, it is 3.3v. The only differences is I add a 500ohm resistor between 5v and VREGIN. &lt;/P&gt;&lt;P&gt;I don't know if it is the reason causing the USB regulator damaged. But it seems it is very easy to break it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2013 19:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243388#M6130</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-12-05T19:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: USB regulator no 3.3v comes out from VOUT33</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243389#M6131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I use another new board and USB regulator part works.&lt;/P&gt;&lt;P&gt;The PC can detect the USB device, but it shows "Unknown devide". I installed the driver from C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\inf.&lt;/P&gt;&lt;P&gt;But it shows me:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41527i508323A75EC21203/image-size/large?v=v2&amp;amp;px=999" title="usb4.png" alt="usb4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas about this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2013 20:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-regulator-no-3-3v-comes-out-from-VOUT33/m-p/243389#M6131</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-12-05T20:36:14Z</dc:date>
    </item>
  </channel>
</rss>