<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 porting MK22FN MCUBOOT SDK middleware to MK21FN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1316866#M61120</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;MCUBOOT is not available for &lt;SPAN&gt;MK21FN as SDK middleware but I wonder if I can get this package for the MK22FN (in this case yes, it's available) and port it to the MK21FN MCU. &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;How difficult would it be?&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance,&lt;BR /&gt;GS&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Aug 2021 18:22:46 GMT</pubDate>
    <dc:creator>gschelotto</dc:creator>
    <dc:date>2021-08-02T18:22:46Z</dc:date>
    <item>
      <title>porting MK22FN MCUBOOT SDK middleware to MK21FN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1316866#M61120</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;MCUBOOT is not available for &lt;SPAN&gt;MK21FN as SDK middleware but I wonder if I can get this package for the MK22FN (in this case yes, it's available) and port it to the MK21FN MCU. &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;How difficult would it be?&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance,&lt;BR /&gt;GS&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Aug 2021 18:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1316866#M61120</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2021-08-02T18:22:46Z</dc:date>
    </item>
    <item>
      <title>Re: porting MK22FN MCUBOOT SDK middleware to MK21FN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1317675#M61134</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27177"&gt;@gschelotto&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I&amp;nbsp; think it wouldn't be very difficult. MK21FN architecture is similar to K22F120M.&amp;nbsp; K21FN has SDK too. So,&lt;/P&gt;
&lt;P&gt;1. use the K21FN SDK toreplace the driver and chip related file.&lt;/P&gt;
&lt;P&gt;2. IO configuration.&lt;/P&gt;
&lt;P&gt;3. maybe some clock&lt;/P&gt;
&lt;P&gt;4. The peripherals which is used for download applications.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 03:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1317675#M61134</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-08-04T03:18:26Z</dc:date>
    </item>
    <item>
      <title>Re: porting MK22FN MCUBOOT SDK middleware to MK21FN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1336534#M61442</link>
      <description>&lt;P&gt;Hi Jing,&lt;/P&gt;&lt;P&gt;I've finally ported the MCU boot to my custom MK21 board following your suggestions. Everything work as expected and it's totally compatible with our CAN tools used for the MK22 ROM Bootloader. Thank you for the given support!&lt;/P&gt;&lt;P&gt;regards,&lt;BR /&gt;gaston&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 06:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/porting-MK22FN-MCUBOOT-SDK-middleware-to-MK21FN/m-p/1336534#M61442</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2021-09-08T06:27:35Z</dc:date>
    </item>
  </channel>
</rss>