<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSRAM size and location for MK64FX512VLL12</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315332#M61104</link>
    <description>&lt;P&gt;Can someone from NXP please confirm the SRAM size and address range for the&amp;nbsp;MK64FX512VLL12?&lt;/P&gt;&lt;P&gt;Per the datasheet, this should be 256KB, but there's conflicting information in the reference manual. The reference manual indicates a size of 256 KB, but address range of&amp;nbsp;0x1FFF_0000-0x2001_FFFF (which is only 192 KB)&lt;/P&gt;&lt;P&gt;See attached picture from the table in section 3.5.3.1 of the latest reference manual v.5.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jul 2021 14:08:29 GMT</pubDate>
    <dc:creator>steve32768</dc:creator>
    <dc:date>2021-07-29T14:08:29Z</dc:date>
    <item>
      <title>SRAM size and location for MK64FX512VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315332#M61104</link>
      <description>&lt;P&gt;Can someone from NXP please confirm the SRAM size and address range for the&amp;nbsp;MK64FX512VLL12?&lt;/P&gt;&lt;P&gt;Per the datasheet, this should be 256KB, but there's conflicting information in the reference manual. The reference manual indicates a size of 256 KB, but address range of&amp;nbsp;0x1FFF_0000-0x2001_FFFF (which is only 192 KB)&lt;/P&gt;&lt;P&gt;See attached picture from the table in section 3.5.3.1 of the latest reference manual v.5.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 14:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315332#M61104</guid>
      <dc:creator>steve32768</dc:creator>
      <dc:date>2021-07-29T14:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: SRAM size and location for MK64FX512VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315422#M61107</link>
      <description>&lt;P&gt;Yes, the MK64FX512VLL12 has 256 KB of SRAM. Still, I will escalate your remarks on the address ranges in the Reference Manual as a possible documentation error and will get back to you as soon as I receive a response.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 17:17:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315422#M61107</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2021-07-29T17:17:34Z</dc:date>
    </item>
    <item>
      <title>Re: SRAM size and location for MK64FX512VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315425#M61108</link>
      <description>&lt;P&gt;Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 17:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315425#M61108</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2021-07-29T17:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: SRAM size and location for MK64FX512VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315426#M61109</link>
      <description>&lt;P&gt;Thanks for the quick reply on that!&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 17:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-size-and-location-for-MK64FX512VLL12/m-p/1315426#M61109</guid>
      <dc:creator>steve32768</dc:creator>
      <dc:date>2021-07-29T17:37:21Z</dc:date>
    </item>
  </channel>
</rss>