<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: 5v Tolerant pins as Open Collector Drivers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303122#M60980</link>
    <description>&lt;P&gt;If get rid of the transistors watch the total package sink current that is allowable on Vss.&lt;BR /&gt;Getting close to that can cause ground bounce problems during load switching,&amp;nbsp;if many outputs transition at the same time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jul 2021 11:58:19 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2021-07-06T11:58:19Z</dc:date>
    <item>
      <title>5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1302583#M60971</link>
      <description>&lt;P&gt;As I was reviewing the datasheets/reference manuals of the MK21FX512VMD12 and MK22FN1M0AVMD12, I noticed that there was the comment that all GPIO pins are 5V tolerant.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Going through the questions about this previously, it seems that only the input functionality of the pins are 5V tolerant, the outputs (even if they are in open drain mode) engage the anti-static diodes to the chip's Vdd and are only tolerant to what Vdd which is a maximum of 3.6V.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my application, I have a number of pins that are driving NPN transistors as open collectors drivers to 5V circuitry and I was wondering:&lt;/P&gt;&lt;P&gt;Could I use the pins as 5V open drain outputs if, when the driver is disabled the pin is in input mode (and is 5V tolerant) and when I want to pull the line low (which the NPN transistor was doing) change to output mode with a low output?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It's certainly no less kludgy than using the NPN transistor, and it saves me $0.05 in each instance.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx!&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jul 2021 20:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1302583#M60971</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-07-05T20:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303122#M60980</link>
      <description>&lt;P&gt;If get rid of the transistors watch the total package sink current that is allowable on Vss.&lt;BR /&gt;Getting close to that can cause ground bounce problems during load switching,&amp;nbsp;if many outputs transition at the same time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 11:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303122#M60980</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-07-06T11:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303243#M60985</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In one case the pins are driving the inputs to a TC74AC138FTEL (CMOS Logic) with an equivalant input of:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="74AC Input Circuit.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/148978i78A22A5C2F383A93/image-size/large?v=v2&amp;amp;px=999" role="button" title="74AC Input Circuit.jpg" alt="74AC Input Circuit.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;74AC Input Circuit.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So I think I can use a 100k for the pull up.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the other case, it's five PNP transistors (MMBTA06LT1G - Hfe of 100) of which only one should be active at any time that will need a maximum of 200mA through it, which means I should be drawing 2mA through it.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;When I do a power inventory, according to the Datasheet, Idd_run (Run mode current - all peripheral clocs enabled, code executing from flash) = 49.9mA (I obviously use 50mA for my calculations).&amp;nbsp; The current application circuit's peripheral total worst case (which &lt;STRONG&gt;shouldn't&lt;/STRONG&gt; happen) current sink from all peripherals active = 103mA.&amp;nbsp; The maximum current draw for normal operation is 84mA.&amp;nbsp; Remove the NPN transistors will drop the worst possible case number to 86mA and the normal operation maximum current sink to 66mA.&amp;nbsp; It also provides me with a cost reduction of about $0.45 per PCB.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Idd (Total sink current for the device) = 185mA so in any case I'm not exceeding the total sink for the device so I think I'm good.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 14:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303243#M60985</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-07-06T14:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303259#M60989</link>
      <description>&lt;P&gt;Yes current sounds reasonable.&lt;BR /&gt;185mA in a small package does fell a bit toasty.&lt;BR /&gt;&lt;BR /&gt;Alas those static protection diodes are there for a reason.&amp;nbsp; It is not clear to me if you are saying you are using the series without the protection diode to Vcc?&amp;nbsp;&amp;nbsp;&lt;BR /&gt;It becomes more of a board handling issue, physically, than run time issue.&lt;BR /&gt;Presumably all the normal anti-static precautions are taken to make that a non-issue.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 14:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303259#M60989</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-07-06T14:49:26Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303300#M60990</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;185mA at 3.3V is 0.61W in this package shouldn't get that "toasty", you're talking 169 mm^2 in area with a large Gnd and 3V3 Plans for heat dissipation - I haven't noticed any real increase in heat around the MCU (and I have been checking it with a thermal imaging camera).&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not sure what you mean by "y&lt;SPAN&gt;ou are using the series without the protection diode to Vcc&lt;/SPAN&gt;" - as I understand it (and it seems to be confirmed in multiple posts to this forum) that in the Kinetis, digital pins (not analog) in &lt;STRONG&gt;input&lt;/STRONG&gt; mode do not have an ESD diode to Vdd.&amp;nbsp; The datasheets have the note:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="5V Tolerant Pins.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/148992i86FC3AA03E29BBC0/image-size/large?v=v2&amp;amp;px=999" role="button" title="5V Tolerant Pins.jpg" alt="5V Tolerant Pins.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;5V Tolerant Pins.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Again, it appears this is the case when the pin is in input mode but not any of the output modes (in those cases there is diode protection to Vdd).&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, the plan is to keep the IO pin in input mode until I need to sink current, at which point I will change the pin to an output (driving a low value).&amp;nbsp; With a current limiting resistor, this should properly simulate an open collector output&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 15:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303300#M60990</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-07-06T15:33:11Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303339#M60991</link>
      <description>&lt;P&gt;I was referring to the Figure 1.2 for the VHC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 17:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303339#M60991</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-07-06T17:16:19Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303348#M60992</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry?&amp;nbsp; I don't know what "VHC" is and none of the NXP documents have a Figure 1.2.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 17:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303348#M60992</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-07-06T17:27:51Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303380#M60993</link>
      <description>&lt;P&gt;I am refereeing to the&amp;nbsp;&lt;SPAN&gt;TC74AC138FTEL image posted above, not the NXP part.&lt;BR /&gt;VHC without static diode to Vcc is on right.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 20:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303380#M60993</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-07-06T20:16:05Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303385#M60994</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry, I should have looked there - I had moved on from the demuxer.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the&amp;nbsp;&lt;SPAN&gt;TC74AC138FTEL (the left side of Figure 1.2), not the VHC.&amp;nbsp; The AC has the ESD diodes in the input so there shouldn't be any worries.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 20:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303385#M60994</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-07-06T20:28:34Z</dc:date>
    </item>
    <item>
      <title>Re: 5v Tolerant pins as Open Collector Drivers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303521#M60996</link>
      <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I modified a prototype PCB by taking out the NPN transistors as detailed here and things worked as expected.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 03:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5v-Tolerant-pins-as-Open-Collector-Drivers/m-p/1303521#M60996</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2021-07-07T03:09:09Z</dc:date>
    </item>
  </channel>
</rss>