<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFailure of Start bit generation in I2C</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failure-of-Start-bit-generation-in-I2C/m-p/1302084#M60954</link>
    <description>&lt;P&gt;What are the possible causes of start bit not being generated in I2C using MK60DX256VLL10 though the same code is running fine when using TWR-K60D100M. In my own PCB,&amp;nbsp;MK60DX256VLL10 drives PCA9698 using I2C but could not get it to work becaue microcontroller is not able to generate start bit. When I use I2C signals of&amp;nbsp;TWR-K60D100M (in which accelerometer is being controlled using I2C) to connect to PCA9698, PCA9698 starts working because now the start bit is being generated. Is there any I2C specific setting to initiate in my controller&amp;nbsp;MK60DX256VLL10 ( some settings to initiate I2C or something like that which is not mentioned in manuals) beacuse I am sucessfully using this controller on my same PCB to make use of its GPIO and CAN ports?&lt;/P&gt;</description>
    <pubDate>Sun, 04 Jul 2021 16:53:35 GMT</pubDate>
    <dc:creator>hfabbasi</dc:creator>
    <dc:date>2021-07-04T16:53:35Z</dc:date>
    <item>
      <title>Failure of Start bit generation in I2C</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failure-of-Start-bit-generation-in-I2C/m-p/1302084#M60954</link>
      <description>&lt;P&gt;What are the possible causes of start bit not being generated in I2C using MK60DX256VLL10 though the same code is running fine when using TWR-K60D100M. In my own PCB,&amp;nbsp;MK60DX256VLL10 drives PCA9698 using I2C but could not get it to work becaue microcontroller is not able to generate start bit. When I use I2C signals of&amp;nbsp;TWR-K60D100M (in which accelerometer is being controlled using I2C) to connect to PCA9698, PCA9698 starts working because now the start bit is being generated. Is there any I2C specific setting to initiate in my controller&amp;nbsp;MK60DX256VLL10 ( some settings to initiate I2C or something like that which is not mentioned in manuals) beacuse I am sucessfully using this controller on my same PCB to make use of its GPIO and CAN ports?&lt;/P&gt;</description>
      <pubDate>Sun, 04 Jul 2021 16:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failure-of-Start-bit-generation-in-I2C/m-p/1302084#M60954</guid>
      <dc:creator>hfabbasi</dc:creator>
      <dc:date>2021-07-04T16:53:35Z</dc:date>
    </item>
    <item>
      <title>Re: Failure of Start bit generation in I2C</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failure-of-Start-bit-generation-in-I2C/m-p/1303415#M60995</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well. I think this issue was solved in this community post: &lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-start-condition-issue/td-p/1298650" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-start-condition-issue/td-p/1298650&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 22:48:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failure-of-Start-bit-generation-in-I2C/m-p/1303415#M60995</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-07-06T22:48:33Z</dc:date>
    </item>
  </channel>
</rss>