<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: RTC Compensation in Kinetis MK22</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/RTC-Compensation-in-Kinetis-MK22/m-p/1296337#M60910</link>
    <description>&lt;P&gt;Hello Vaibhavi,&lt;/P&gt;
&lt;P&gt;I haven’t seen the the TCR and CIR calculation using the 1Hz signal instead of 32.768KHz but the overall process would be similar as the one described in AN4949.&lt;/P&gt;
&lt;P&gt;As for the precision of the measurement, an increased resolution would lead to a finer compensation up to the actual resolution of the TCR and CIR, so in theory there would be a point in which a finer compensation would not be possible, but these registers allow for a very fine compensation that suits most application.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
    <pubDate>Tue, 22 Jun 2021 19:13:46 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2021-06-22T19:13:46Z</dc:date>
    <item>
      <title>RTC Compensation in Kinetis MK22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/RTC-Compensation-in-Kinetis-MK22/m-p/1285180#M60673</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using custom board using MK22FX512AVLQ12. I am using RTC of the controller with external crystal of 32.768KHz. As the crystal frequency will not be this exact value, I am performing RTC compensation to avoid lag in RTC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have already referred to&amp;nbsp;&lt;LI-MESSAGE title="How to Use the Kinetis RTC Time Compensation Register (RTC_TCR)?" uid="757101" url="https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Use-the-Kinetis-RTC-Time-Compensation-Register-RTC-TCR/m-p/757101#U757101" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-forum-thread lia-fa-icon lia-fa-forum lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;and I am able to perform the compensation by measuring RTC clock_out of 32.768KHz with a resolution of 0.1Hz.&lt;/P&gt;&lt;P&gt;But I am not sure how the precision in measurement of frequency will affect my values of TCR and CIR. How accurately should I measure the frequency for calculating the values of TCR and CIR? What would be the effect on those value if I measure the frequency with resolution of 1Hz vs 0.1Hz vs 0.01Hz?&lt;/P&gt;&lt;P&gt;Also I would like to know how can I calculate values of TCR and CIR using 1Hz signal on CLOCK_OUT instead of 32.768KHz?&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Vaibhavi&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 07:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/RTC-Compensation-in-Kinetis-MK22/m-p/1285180#M60673</guid>
      <dc:creator>vaibhavi_padwal</dc:creator>
      <dc:date>2021-06-01T07:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: RTC Compensation in Kinetis MK22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/RTC-Compensation-in-Kinetis-MK22/m-p/1296337#M60910</link>
      <description>&lt;P&gt;Hello Vaibhavi,&lt;/P&gt;
&lt;P&gt;I haven’t seen the the TCR and CIR calculation using the 1Hz signal instead of 32.768KHz but the overall process would be similar as the one described in AN4949.&lt;/P&gt;
&lt;P&gt;As for the precision of the measurement, an increased resolution would lead to a finer compensation up to the actual resolution of the TCR and CIR, so in theory there would be a point in which a finer compensation would not be possible, but these registers allow for a very fine compensation that suits most application.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 19:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/RTC-Compensation-in-Kinetis-MK22/m-p/1296337#M60910</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-06-22T19:13:46Z</dc:date>
    </item>
  </channel>
</rss>