<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: How do the on chip True Random Number Generators work?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1289662#M60803</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;TRNG is based on collecting bits from a random noise source. This random noise source is a ring oscillator that is sensitive to random noise (temperature variations, voltage variations, cross-talk and other random noise) within the device in which the TRNG is used. TRNG can be used to seed a hardware or software based implementation of a DRBG defined by SP800-90.&lt;/P&gt;
&lt;P&gt;TRNG hasn't been certified with FIPS and there are no plans to do it for KINETIS.&lt;/P&gt;
&lt;P&gt;But, the TRNG is designed in accordance with SP800-90B guidelines, if you combine it with a SW DRBG (per SP800-90B guidelines), it should meet the FIPS requirements.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 06:38:13 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-06-09T06:38:13Z</dc:date>
    <item>
      <title>How do the on chip True Random Number Generators work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1287513#M60735</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Several NXP chips have added True Random Number Generators.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I really would like to see some data from NXP on how it works and what NIST tests its has passed.&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I know what some places do is take a mediocre&amp;nbsp;noise source and run it through a hash algorithm&amp;nbsp;to make it appear better than it truly is.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Any true random process will also make a really good thermometer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Take a look at the Random Number section:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://www.schneier.com/academic/" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.schneier.com/academic/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 11:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1287513#M60735</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-06-04T11:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: How do the on chip True Random Number Generators work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1289662#M60803</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38376"&gt;@bobpaddock&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;TRNG is based on collecting bits from a random noise source. This random noise source is a ring oscillator that is sensitive to random noise (temperature variations, voltage variations, cross-talk and other random noise) within the device in which the TRNG is used. TRNG can be used to seed a hardware or software based implementation of a DRBG defined by SP800-90.&lt;/P&gt;
&lt;P&gt;TRNG hasn't been certified with FIPS and there are no plans to do it for KINETIS.&lt;/P&gt;
&lt;P&gt;But, the TRNG is designed in accordance with SP800-90B guidelines, if you combine it with a SW DRBG (per SP800-90B guidelines), it should meet the FIPS requirements.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 06:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1289662#M60803</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-06-09T06:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: How do the on chip True Random Number Generators work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1289897#M60806</link>
      <description>&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 12:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-the-on-chip-True-Random-Number-Generators-work/m-p/1289897#M60806</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-06-09T12:05:24Z</dc:date>
    </item>
  </channel>
</rss>