<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MK60DN512ZVLQ10 4N30D Reset Problem in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160626#M608</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale Italy confirmed us that Freescale has found too this problem on 4N30D mask set and it will be corrected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Revised errata sheet of the 4N30D will be realised in the following days .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 May 2012 13:53:13 GMT</pubDate>
    <dc:creator>GottiLuca</dc:creator>
    <dc:date>2012-05-10T13:53:13Z</dc:date>
    <item>
      <title>MK60DN512ZVLQ10 4N30D Reset Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160625#M607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We've done a custom board with MK60DN512ZVLQ10&amp;nbsp; ( 144 pin LQFP version ), mask set 4N30D installed.&lt;/P&gt;&lt;P&gt;Mask set 4N30D should be the INITIAL production mask set , so really close to the definitive one ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, we've seen a problem when powering the 3,3 V supply with a ramp time less of 2 ms ( something that could happen for example if u're using the micro for a USB device , but not only in this case ) : the microcontroller simply doesn't reset itself&amp;nbsp; .&lt;/P&gt;&lt;P&gt;We've also tried to add an external reset generator ( like MAX809 ) but nothing : if 3,3 V supply is too "fast" the micro doesn't start. The polite thing is that if we , after power up event ( even 2 ms after ) , reset the part by an external reset switch, the&lt;/P&gt;&lt;P&gt;part starts.&lt;/P&gt;&lt;P&gt;After struggling our minds for some days with this problem, at the end we've tried to install the very same pcb a PK60N512VLQ10 with mask code 0M33Z ( the initial mask set !!! ) and , magically, problem disappeared !!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, our conclusion is that on mask set 4N30D there is this very annoying problem !!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;( probably the problem it is related to the POR module and / or reset logic )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2012 16:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160625#M607</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2012-05-08T16:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: MK60DN512ZVLQ10 4N30D Reset Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160626#M608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale Italy confirmed us that Freescale has found too this problem on 4N30D mask set and it will be corrected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Revised errata sheet of the 4N30D will be realised in the following days .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2012 13:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160626#M608</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2012-05-10T13:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: MK60DN512ZVLQ10 4N30D Reset Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160627#M609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After further investigation, it appears that my REAL problem was caused by a sporious NMI interrupt triggered before system init.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To confirm that we've done a very simple test : we've connected the NMI pin directly to Vdd and problem disappears .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 May 2012 21:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512ZVLQ10-4N30D-Reset-Problem/m-p/160627#M609</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2012-05-11T21:33:31Z</dc:date>
    </item>
  </channel>
</rss>