<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKV31F256 2 Stop Bits in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F256-2-Stop-Bits/m-p/1287896#M60759</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Refer to the RM, the uart only supports one stop bit. The data length can be 8 or 9. So you are right. We do not have 2 stop bit feature.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="uart.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146363i241CFC6978F19820/image-size/medium?v=v2&amp;amp;px=400" role="button" title="uart.PNG" alt="uart.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;uart.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jun 2021 02:15:46 GMT</pubDate>
    <dc:creator>nxf56274</dc:creator>
    <dc:date>2021-06-07T02:15:46Z</dc:date>
    <item>
      <title>MKV31F256 2 Stop Bits</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F256-2-Stop-Bits/m-p/1287648#M60738</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have to use UART1 with&amp;nbsp; 8N2.&amp;nbsp; -&amp;gt;&amp;nbsp; 2 stop bits&lt;/P&gt;&lt;P&gt;Maybe i am blind, but i can't find any µC register for that.&lt;/P&gt;&lt;P&gt;Is it true, that the microcontroller doesn't have this feature?&lt;/P&gt;&lt;P&gt;If yes, is there a work arround?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 16:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F256-2-Stop-Bits/m-p/1287648#M60738</guid>
      <dc:creator>andreasruetten</dc:creator>
      <dc:date>2021-06-04T16:14:38Z</dc:date>
    </item>
    <item>
      <title>Re: MKV31F256 2 Stop Bits</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F256-2-Stop-Bits/m-p/1287896#M60759</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Refer to the RM, the uart only supports one stop bit. The data length can be 8 or 9. So you are right. We do not have 2 stop bit feature.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="uart.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146363i241CFC6978F19820/image-size/medium?v=v2&amp;amp;px=400" role="button" title="uart.PNG" alt="uart.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;uart.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 02:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F256-2-Stop-Bits/m-p/1287896#M60759</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-06-07T02:15:46Z</dc:date>
    </item>
  </channel>
</rss>