<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: There is a way to program k22 via uart2?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/There-is-a-way-to-program-k22-via-uart2/m-p/1286746#M60705</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83531"&gt;@mangramarco&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;yes, you can use the KBOOT for this (see &lt;A href="https://mcuoneclipse.com/2018/03/03/flash-resident-usb-hid-bootloader-with-the-nxp-kinetis-k22-microcontroller/" target="_blank"&gt;https://mcuoneclipse.com/2018/03/03/flash-resident-usb-hid-bootloader-with-the-nxp-kinetis-k22-microcontroller/&lt;/A&gt; where I used it with USB CDC). That bootloader from NXP supports different loading interfaces like USB, SPI, I2C and as well UART.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 10:31:07 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2021-06-03T10:31:07Z</dc:date>
    <item>
      <title>There is a way to program k22 via uart2?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/There-is-a-way-to-program-k22-via-uart2/m-p/1286732#M60704</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i've a board with k22 mcu. This communicate with other mcu by means of uart2 and there is not any other external communication implemented. I want to update the firmware of k22 passing through other mcu. Is it possible?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 10:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/There-is-a-way-to-program-k22-via-uart2/m-p/1286732#M60704</guid>
      <dc:creator>mangramarco</dc:creator>
      <dc:date>2021-06-03T10:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: There is a way to program k22 via uart2?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/There-is-a-way-to-program-k22-via-uart2/m-p/1286746#M60705</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83531"&gt;@mangramarco&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;yes, you can use the KBOOT for this (see &lt;A href="https://mcuoneclipse.com/2018/03/03/flash-resident-usb-hid-bootloader-with-the-nxp-kinetis-k22-microcontroller/" target="_blank"&gt;https://mcuoneclipse.com/2018/03/03/flash-resident-usb-hid-bootloader-with-the-nxp-kinetis-k22-microcontroller/&lt;/A&gt; where I used it with USB CDC). That bootloader from NXP supports different loading interfaces like USB, SPI, I2C and as well UART.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 10:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/There-is-a-way-to-program-k22-via-uart2/m-p/1286746#M60705</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-06-03T10:31:07Z</dc:date>
    </item>
  </channel>
</rss>