<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL16Z32M4</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16Z32M4/m-p/1286491#M60701</link>
    <description>&lt;P&gt;Hi Richard,&lt;/P&gt;
&lt;P&gt;There are many fact may cause kinetis device locked. Please refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F512-is-locked-in-secure-state/m-p/639140?commentID=857127#comment-857127" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F512-is-locked-in-secure-state/m-p/639140?commentID=857127#comment-857127&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 02:37:27 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-06-03T02:37:27Z</dc:date>
    <item>
      <title>KL16Z32M4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16Z32M4/m-p/1286314#M60699</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We have a technical issue with our cpu KL16Z32M4.&lt;/P&gt;&lt;P&gt;We produced more than 10&amp;nbsp;000 units.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The cpu was programmed on each circuit. After sending it to the customer, Some of them stop working.&lt;/P&gt;&lt;P&gt;An investigation on the circuits shows that the cpu is secured although it seems like if there is nothing (as a program) inside it!&lt;/P&gt;&lt;P&gt;What can be the roots causes ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 19:45:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16Z32M4/m-p/1286314#M60699</guid>
      <dc:creator>Richard011</dc:creator>
      <dc:date>2021-06-02T19:45:53Z</dc:date>
    </item>
    <item>
      <title>Re: KL16Z32M4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16Z32M4/m-p/1286491#M60701</link>
      <description>&lt;P&gt;Hi Richard,&lt;/P&gt;
&lt;P&gt;There are many fact may cause kinetis device locked. Please refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F512-is-locked-in-secure-state/m-p/639140?commentID=857127#comment-857127" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F512-is-locked-in-secure-state/m-p/639140?commentID=857127#comment-857127&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 02:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16Z32M4/m-p/1286491#M60701</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-06-03T02:37:27Z</dc:date>
    </item>
  </channel>
</rss>