<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Silicon versions for MK10 processor</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Silicon-versions-for-MK10-processor/m-p/1286436#M60700</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The 'initial' means that it is the 1.x&amp;nbsp;&lt;SPAN&gt;silicon. 'main' means that it is the 2.x silicon. You can refer this &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN4445.pdf" target="_self"&gt;document&lt;/A&gt;. If possible, please do not use the old silicon.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 01:54:43 GMT</pubDate>
    <dc:creator>nxf56274</dc:creator>
    <dc:date>2021-06-03T01:54:43Z</dc:date>
    <item>
      <title>Silicon versions for MK10 processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Silicon-versions-for-MK10-processor/m-p/1286270#M60697</link>
      <description>&lt;P&gt;I need to purchase some MK10DX256VLQ10 processors but none are available atm.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;MK10DX256ZVLQ10 is available but it is using "initial" silicon instead of "main" silicon.&lt;/P&gt;&lt;P&gt;Does anyone know what the difference is between these two versions of silicon and whether the&amp;nbsp;MK10DX256ZVLQ10 is a suitable replacement for the&amp;nbsp;MK10DX256VLQ10?&lt;/P&gt;&lt;P&gt;Any help would be much appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 17:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Silicon-versions-for-MK10-processor/m-p/1286270#M60697</guid>
      <dc:creator>danlowe</dc:creator>
      <dc:date>2021-06-02T17:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: Silicon versions for MK10 processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Silicon-versions-for-MK10-processor/m-p/1286436#M60700</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The 'initial' means that it is the 1.x&amp;nbsp;&lt;SPAN&gt;silicon. 'main' means that it is the 2.x silicon. You can refer this &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN4445.pdf" target="_self"&gt;document&lt;/A&gt;. If possible, please do not use the old silicon.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 01:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Silicon-versions-for-MK10-processor/m-p/1286436#M60700</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-06-03T01:54:43Z</dc:date>
    </item>
  </channel>
</rss>