<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCan Bus message receive rate</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1279060#M60572</link>
    <description>&lt;P&gt;Hey Guys,&lt;/P&gt;&lt;P&gt;i have a Question regarding the can bus rate of receiving from different nodes. At the moment i am using a K60D100M and FRDM-K64 to send Can Messages to a RT1064-EVK. Therefor i edited the "flexcan_interrupt_transfer" example on all 3 of them and set the k60 and k64 to mode A and the 1064 to mode B. I also extendet the rx filter on the 1064 to recieve from two devices and i am able to recieve messages and the id's. But when sending from both in a loop I have to implement a __asm("NOP") command for like 1 million cycles to slow both sending Nodes down. By shortening the sleep time the 1064 starts to crash. So is there a like a buffer which gets clogged or a limit on the recieving side? Cause when looking at the CAN line with an Oscilloscope there is plenty of bandwith left. also changing the baudrate to a higher one doesnt change the crashing. So I guess the limiting part is on the 1064. Has someone an Idea?&lt;/P&gt;&lt;P&gt;Baudrate 25.000 - 250.000&lt;BR /&gt;NOP 1.000.000 per TX&lt;BR /&gt;frame.length = 2 per TX&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Wed, 19 May 2021 14:47:37 GMT</pubDate>
    <dc:creator>Dannii</dc:creator>
    <dc:date>2021-05-19T14:47:37Z</dc:date>
    <item>
      <title>Can Bus message receive rate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1279060#M60572</link>
      <description>&lt;P&gt;Hey Guys,&lt;/P&gt;&lt;P&gt;i have a Question regarding the can bus rate of receiving from different nodes. At the moment i am using a K60D100M and FRDM-K64 to send Can Messages to a RT1064-EVK. Therefor i edited the "flexcan_interrupt_transfer" example on all 3 of them and set the k60 and k64 to mode A and the 1064 to mode B. I also extendet the rx filter on the 1064 to recieve from two devices and i am able to recieve messages and the id's. But when sending from both in a loop I have to implement a __asm("NOP") command for like 1 million cycles to slow both sending Nodes down. By shortening the sleep time the 1064 starts to crash. So is there a like a buffer which gets clogged or a limit on the recieving side? Cause when looking at the CAN line with an Oscilloscope there is plenty of bandwith left. also changing the baudrate to a higher one doesnt change the crashing. So I guess the limiting part is on the 1064. Has someone an Idea?&lt;/P&gt;&lt;P&gt;Baudrate 25.000 - 250.000&lt;BR /&gt;NOP 1.000.000 per TX&lt;BR /&gt;frame.length = 2 per TX&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 14:47:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1279060#M60572</guid>
      <dc:creator>Dannii</dc:creator>
      <dc:date>2021-05-19T14:47:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can Bus message receive rate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1281962#M60613</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186796"&gt;@Dannii&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I think it shouldn't need all the NOPs since the capabilities to receive using in a bus at 250 kbps is much higher than two bytes per node. Some things to check is that all the devices are at the same baud-rate and the same sampling point.&lt;/P&gt;
&lt;P&gt;The only thing is that if you're using the same mailbox and two messages are coming consecutively and the mailbox is not free could cause some unexpected behavior. I will suggest to configure two mailboxes and check if this fix the issue.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 16:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1281962#M60613</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-05-25T16:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: Can Bus message receive rate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1283341#M60638</link>
      <description>&lt;P&gt;Yes Thank you! The&amp;nbsp;&lt;SPAN&gt;two messages are coming consecutively&amp;nbsp;were the problem.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your help!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Daniel&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 09:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Bus-message-receive-rate/m-p/1283341#M60638</guid>
      <dc:creator>Dannii</dc:creator>
      <dc:date>2021-05-27T09:27:02Z</dc:date>
    </item>
  </channel>
</rss>