<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Connection-between-a-TWR-K60D100M-and-MIMXRT1064-EVK/m-p/1278308#M60567</link>
    <description>&lt;P&gt;The Baudrate was the only problem and I fixed it by just changing it in the default settings.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 18 May 2021 14:42:13 GMT</pubDate>
    <dc:creator>Dannii</dc:creator>
    <dc:date>2021-05-18T14:42:13Z</dc:date>
    <item>
      <title>CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Connection-between-a-TWR-K60D100M-and-MIMXRT1064-EVK/m-p/1278138#M60562</link>
      <description>&lt;P&gt;Hey guys,&lt;/P&gt;&lt;P&gt;when connecting the Boards togehter through their CAN Ports and using a Driver for the K60 both seem to work when checking it with an Oscilloscope, but when using the Flexcan example it seems to be not working. Maybe I would guess it is related to the Baudrate because in the exmaple they are on two different ones. But I probably need some help changing the baudrate and maybe other values to connect the devices. When using a TWR-K64 with the 1064 it works like it should but they are configured the same way in the example.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 09:38:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Connection-between-a-TWR-K60D100M-and-MIMXRT1064-EVK/m-p/1278138#M60562</guid>
      <dc:creator>Dannii</dc:creator>
      <dc:date>2021-05-18T09:38:56Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Connection-between-a-TWR-K60D100M-and-MIMXRT1064-EVK/m-p/1278308#M60567</link>
      <description>&lt;P&gt;The Baudrate was the only problem and I fixed it by just changing it in the default settings.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 14:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Connection-between-a-TWR-K60D100M-and-MIMXRT1064-EVK/m-p/1278308#M60567</guid>
      <dc:creator>Dannii</dc:creator>
      <dc:date>2021-05-18T14:42:13Z</dc:date>
    </item>
  </channel>
</rss>