<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-K60D100M no CAN output in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1278127#M60561</link>
    <description>&lt;P&gt;Thank you for your detailed answer.&lt;/P&gt;&lt;P&gt;I did it exactly like you and bevore I always used the console output from the MCUXpresso IDE. But after switching to the terminal everything seems to work! Kinda weired but its working now!&lt;/P&gt;</description>
    <pubDate>Tue, 18 May 2021 09:19:40 GMT</pubDate>
    <dc:creator>Dannii</dc:creator>
    <dc:date>2021-05-18T09:19:40Z</dc:date>
    <item>
      <title>TWR-K60D100M no CAN output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1277664#M60548</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i hava an issue with the K60D100M development board using the CAN connection. I used an Waveshare SN65HVD230 CAN board and connected it to the J11 connector side B Pin 41 and 42. When using the "flexcan interrupt transfer" example&amp;nbsp; it doesn't even send anything over the pins on the development board. Is there a possibility, that the pins I used might be wrong for the example. Cause I can't even measure anything at the 2 pin except a DC voltage around 3.3V on the TX pin (B42). Also is there a specific Jumper to have set that it works?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 14:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1277664#M60548</guid>
      <dc:creator>Dannii</dc:creator>
      <dc:date>2021-05-17T14:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60D100M no CAN output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1277869#M60554</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Daniel,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;I don't have SN65HVD230 CAN board on hand, so I measure the waveform at B42(CAN TX) of J11.&lt;BR /&gt;Since I did not connect external CAN Transceiver on bus, so the waveform will be like this:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NewFile0.bmp" style="width: 320px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144894i727BCE89052B7A15/image-size/large?v=v2&amp;amp;px=999" role="button" title="NewFile0.bmp" alt="NewFile0.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;NewFile0.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you measure the DC voltage by using multimeter, then the voltage may be 3.3v. But you should observe the waveform by using oscilloscope instead of using multimeter.&lt;/P&gt;
&lt;P&gt;I test it on TWR-K60D100M board and select Node A through serial terminal then trigger transmission.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="twrk60d100m_driver_examples_flexcan_interrupt_transfer.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144895i341395912F12105A/image-size/large?v=v2&amp;amp;px=999" role="button" title="twrk60d100m_driver_examples_flexcan_interrupt_transfer.jpg" alt="twrk60d100m_driver_examples_flexcan_interrupt_transfer.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;twrk60d100m_driver_examples_flexcan_interrupt_transfer.jpg&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="select Node A and then trigger transmission.jpg" style="width: 777px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144896i940DB5566E406B81/image-size/large?v=v2&amp;amp;px=999" role="button" title="select Node A and then trigger transmission.jpg" alt="select Node A and then trigger transmission.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;select Node A and then trigger transmission.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="B42.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144897iE9DCA267BE006231/image-size/large?v=v2&amp;amp;px=999" role="button" title="B42.jpg" alt="B42.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;B42.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 02:37:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1277869#M60554</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-05-18T02:37:23Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60D100M no CAN output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1278127#M60561</link>
      <description>&lt;P&gt;Thank you for your detailed answer.&lt;/P&gt;&lt;P&gt;I did it exactly like you and bevore I always used the console output from the MCUXpresso IDE. But after switching to the terminal everything seems to work! Kinda weired but its working now!&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 09:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-no-CAN-output/m-p/1278127#M60561</guid>
      <dc:creator>Dannii</dc:creator>
      <dc:date>2021-05-18T09:19:40Z</dc:date>
    </item>
  </channel>
</rss>