<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MFS library read on SDHC card very slow</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MFS-library-read-on-SDHC-card-very-slow/m-p/1277089#M60537</link>
    <description>&lt;P&gt;When I was using the fread function the parameter "Size of element to be read" was set to one. When use a larger value for "Size of element to be read" the reads are much faster. Know it takes me ~1.5 milliseconds to read&amp;nbsp;4,380 bytes&lt;/P&gt;</description>
    <pubDate>Fri, 14 May 2021 17:29:19 GMT</pubDate>
    <dc:creator>MattJCole</dc:creator>
    <dc:date>2021-05-14T17:29:19Z</dc:date>
    <item>
      <title>MFS library read on SDHC card very slow</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MFS-library-read-on-SDHC-card-very-slow/m-p/1275094#M60499</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am using. KSDK Version: 1.3.0, MFS library (not sure which one): ,Processor: MK65FN2M0xxx18&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The read speed from an SDHC card is very slow. For every 1460 bytes read it takes 60&amp;nbsp;&lt;/SPAN&gt;milliseconds. I can not figure out why it is taking so long. I know I am not giving much information I do not know what I am missing. When I looked at the setup of the SD card using the debugger the data width is 4 bits not 1 bit and the baud rate is set to 25 MHz. Is there a setting or settings I need to set to speed up the reading of the SD card.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 May 2021 15:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MFS-library-read-on-SDHC-card-very-slow/m-p/1275094#M60499</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2021-05-11T15:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: MFS library read on SDHC card very slow</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MFS-library-read-on-SDHC-card-very-slow/m-p/1277089#M60537</link>
      <description>&lt;P&gt;When I was using the fread function the parameter "Size of element to be read" was set to one. When use a larger value for "Size of element to be read" the reads are much faster. Know it takes me ~1.5 milliseconds to read&amp;nbsp;4,380 bytes&lt;/P&gt;</description>
      <pubDate>Fri, 14 May 2021 17:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MFS-library-read-on-SDHC-card-very-slow/m-p/1277089#M60537</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2021-05-14T17:29:19Z</dc:date>
    </item>
  </channel>
</rss>