<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM-KV31f Thermistor</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KV31f-Thermistor/m-p/1271831#M60449</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the part number of the thermistor on the FRDM-KV31f?&lt;/P&gt;&lt;P&gt;Also, how do I turn the output voltage for THER_A and THER_B (schematic page 3) into a temperature? I've read about the B constant, V_in, and resistances. I'm not sure what the capacitors do. I'm not sure why the circuit has what looks like 2 voltage dividers - one for THER_A and one for THER_B. I'm also not sure why&amp;nbsp; there are resistors (R47 and R46) between the thermistors and the ADC. If anyone could provide some insight into these things, it would be appreciated.&lt;/P&gt;</description>
    <pubDate>Tue, 04 May 2021 16:52:37 GMT</pubDate>
    <dc:creator>Kane_Lee</dc:creator>
    <dc:date>2021-05-04T16:52:37Z</dc:date>
    <item>
      <title>FRDM-KV31f Thermistor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KV31f-Thermistor/m-p/1271831#M60449</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the part number of the thermistor on the FRDM-KV31f?&lt;/P&gt;&lt;P&gt;Also, how do I turn the output voltage for THER_A and THER_B (schematic page 3) into a temperature? I've read about the B constant, V_in, and resistances. I'm not sure what the capacitors do. I'm not sure why the circuit has what looks like 2 voltage dividers - one for THER_A and one for THER_B. I'm also not sure why&amp;nbsp; there are resistors (R47 and R46) between the thermistors and the ADC. If anyone could provide some insight into these things, it would be appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 16:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KV31f-Thermistor/m-p/1271831#M60449</guid>
      <dc:creator>Kane_Lee</dc:creator>
      <dc:date>2021-05-04T16:52:37Z</dc:date>
    </item>
  </channel>
</rss>