<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKW21Z to replace KW41Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW21Z-to-replace-KW41Z/m-p/1270168#M60424</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I need to make a production, and I currently use a KW41Z. Of course, it's near impossible to find any stock, and the lead time is now 52 weeks.&lt;/P&gt;&lt;P&gt;I only use the SMAC 802.15.4 stack, so it seems I can use the KW21Z as a drop in replacement. Can you confirm that it is a direct replacement?&lt;/P&gt;&lt;P&gt;Should I change the init vector (or other stuff?), and is the SMAC stack still compatible (I just modified it a bit to not use the common library and call directly my freertos routine, but the core of the library has not changed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Matthieu&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Apr 2021 07:52:26 GMT</pubDate>
    <dc:creator>paralax</dc:creator>
    <dc:date>2021-04-29T07:52:26Z</dc:date>
    <item>
      <title>KW21Z to replace KW41Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW21Z-to-replace-KW41Z/m-p/1270168#M60424</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I need to make a production, and I currently use a KW41Z. Of course, it's near impossible to find any stock, and the lead time is now 52 weeks.&lt;/P&gt;&lt;P&gt;I only use the SMAC 802.15.4 stack, so it seems I can use the KW21Z as a drop in replacement. Can you confirm that it is a direct replacement?&lt;/P&gt;&lt;P&gt;Should I change the init vector (or other stuff?), and is the SMAC stack still compatible (I just modified it a bit to not use the common library and call directly my freertos routine, but the core of the library has not changed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Matthieu&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 07:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW21Z-to-replace-KW41Z/m-p/1270168#M60424</guid>
      <dc:creator>paralax</dc:creator>
      <dc:date>2021-04-29T07:52:26Z</dc:date>
    </item>
    <item>
      <title>Re: KW21Z to replace KW41Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW21Z-to-replace-KW41Z/m-p/1270985#M60432</link>
      <description>&lt;P&gt;Hi Matthieu,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Yes, you can use the KW21Z if you are interested in 802.15.4.&lt;/P&gt;
&lt;P&gt;Just be sure to buy the same Package, Flash and SRAM version.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Ricardo_Zamora_1-1619808560472.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/143752i82B28B2A1B366355/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ricardo_Zamora_1-1619808560472.png" alt="Ricardo_Zamora_1-1619808560472.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ricardo_Zamora_1-1619808560472.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 18:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW21Z-to-replace-KW41Z/m-p/1270985#M60432</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-04-30T18:50:18Z</dc:date>
    </item>
  </channel>
</rss>